Supplier eBooks

Vishay - An Automotive Grade Above

Issue link: https://resources.mouser.com/i/1429079

Contents of this Issue

Navigation

Page 8 of 27

mouser.com/vishay / 9 The design features two sets of MOSFETs (TR2/TR3 in Figure 2) connected in a bi-directional arrangement to handle the high load current. Without this type of connection, the current could flow back through the MOSFET body diode to the battery when the load is deactivated. Each switch requires 10 Vishay SQJQ160E MOSFETs connected in parallel to minimize resistance and power dissipation. With this arrangement, total losses can be limited to ~10W at 200A operation. To prevent greater damage to the load and protect the vehicle wiring in case of a short circuit, the load current is continuously measured using the shunt resistor R2 in Figure 2 (4x the Vishay WSLP3921 300µΩ in parallel). When a defined overload current is detected, the controller can quickly disconnect the battery from the short- circuited load. Until the load is deactivated during this short amount of time, the eFuse can handle a considerable amount of overload current because of the high pulse drain current capability of the bond wireless MOSFETs. Also, the continuous current measurement is used by the vehicle's body control module (via serial interface) to monitor the state of health (charge level, remaining lifetime, etc.) of the battery. Another common issue that occurs when first connecting the battery to the load during vehicle start-up is the potential in-rush current because of any uncharged capacitor banks in the load. If this resulting high peak current is allowed to occur, downstream components could be damaged, and battery life could be reduced. Therefore, a pre-charge circuit must be used to limit the in-rush current to an acceptable level. Learn More Learn More D2TO20 Series SMD Power Resistors XMC7K24CA XClampR™ TVS Diodes In this design, a Vishay SQJA84E MOSFET (TR1 in Figure 2), a Vishay VSS8D5M6 Schottky diode and a Vishay D2TO20 resistor (R1 in Figure 2) are used to limit the in-rush current to a maximum of 5A at 48V. This thick film resistor provides superior power handling and heat conduction due to physical construction and an integrated heatsink. Before energizing the load, TR1 is switched on for a predefined time (10ms), and the output voltage X3 in Figure 2 is monitored. If the output voltage has not reached ~90% of the input voltage after that time, the process is terminated, assuming a short circuit in the load or wiring. If the output has reached the appropriate level, then TR1 is switched off, and TR2/TR3 is switched on to energize the load. Note that the Schottky diode is used to prevent backflow of the current through the MOSFET body diode when it is off. In terms of protection features, a Vishay NTCS0805 (NTC1 in Figure 2), featuring polymer terminations for superior mechanical reliability under thermal stress, is used to monitor the temperature, and Vishay XMC7K24CA and 5KASMC30A transient voltage suppressors are connected in series (D1a and D1b in Figure 2) to protect the components against transients from the vehicle load. A novel electronic switch and resettable fuse design has been presented that can be used in any 48V load application up to 200A and replace mechanical relays that are prone to excessive arcing and shorter lifetimes. ▼ Figure 2: The eFuse power stage as shown in a simplified schematic. (Source: Vishay)

Articles in this issue

Links on this page

view archives of Supplier eBooks - Vishay - An Automotive Grade Above