Supplier eBooks

Samtec - Flyover ® Solutions Break Next-Gen System Architecture Constraints

Issue link: https://resources.mouser.com/i/1495600

Contents of this Issue

Navigation

Page 6 of 23

can achieve 64 Gbps pulse amplitude modulation 4-level (PAM4) data rates. Although both are considered high- speed in their specific industries, the vast difference in speed between the two shows how the term "high-speed" is used somewhat loosely. But, if considering all applications across all industries, the highest speeds currently used are around 112 Gbps PAM4, which are significantly higher than those used in everyday applications. To achieve such speeds, engineers must use several different techniques including double data rate (whereby a single clock cycle transmits data on the rising and falling edge) and advanced modulation schemes like PAM4, which encodes two bits of logic per signal level. Even with these techniques deployed, the frequency of signals can easily exceed the 30 GHz range, which introduces many challenges from PCB signal routing to the cable assembly used to transmit such signals. Applications that use such high speeds are often at the bleeding edge of technology, including artificial intelligence (AI), machine learning, high-performance computing (HPC), and data centers. In all these applications, compute platforms are found in racks that use high-speed input/output to move data from servers to storage units and then across entire networks of other clustered systems. As the maximum speed of such a system is often defined by its weakest link, engineers are challenged to optimize channel and system performance. C h a p t e r 1 | D e f i n i n g " H i g h - S p e e d " Ve r s u s H i g h - S p e e d Matthew Burns Technical Marketing Manager, Samtec Some of the common high-speed applications where Samtec focuses a lot of attention are data center applications, networking, servers, memory, AI systems, HPC, and supercomputing." 7 Samtec Flyover ® Solutions Break Next-Gen System Architecture Constraints

Articles in this issue

Links on this page

view archives of Supplier eBooks - Samtec - Flyover ® Solutions Break Next-Gen System Architecture Constraints