Supplier eBooks

Samtec - Flyover ® Solutions Break Next-Gen System Architecture Constraints

Issue link: https://resources.mouser.com/i/1495600

Contents of this Issue

Navigation

Page 18 of 23

Copper cable assemblies are generally limited to meters or hundreds of meters. But for fiber optics, depending on the type of cable used, the fiber optic transceiver distances can be hundreds to thousands of meters without suffering signal integrity issues. When compared to copper cables, fiber optic cables offer around 1,000 times more bandwidth." Benjamin Grab Manager, Applications Engineering Team, Optical Group, Samtec C h a p t e r 5 While copper cable assemblies have been the primary means of communication in electronics since the first circuits were conceived, future electronic systems will leverage the many advantages of optical systems. For example, multiple wavelengths can use the same transfer medium without interfering, thus offering extremely high bandwidths. Another major benefit to fiber optic systems is that they are significantly lighter than copper cable assemblies, which allows for more compact bundles. This lower weight also allows designs to be reduced in mass, which is important for applications where weight is a design constraint (e.g., the aerospace industry). Additionally, as light is itself fundamental, a fiber optic cable can theoretically handle any future communication system—fiber optic systems are APPROACHING LIGHT SPEED 19 Samtec Flyover ® Solutions Break Next-Gen System Architecture Constraints

Articles in this issue

Links on this page

view archives of Supplier eBooks - Samtec - Flyover ® Solutions Break Next-Gen System Architecture Constraints