Supplier eBooks

Samtec - Flyover ® Solutions Break Next-Gen System Architecture Constraints

Issue link: https://resources.mouser.com/i/1495600

Contents of this Issue

Navigation

Page 8 of 23

Anthony Fellbaum Senior FAE and BDM - Canada, Samtec C h a p t e r 2 When creating PCBs designed to handle signals up to 112 Gbps PAM4, engineers face monumental challenges that may be extremely difficult to solve. In fact, engineers could solve one challenge but create a new one in the solution they develop. From getting data out of a silicon device to having those data arrive at their destination, high-speed signals bring grief at every stage of the journey. Signal frequency is by far the biggest factor in signal integrity. As the frequency of a signal increases, that signal can radiate energy through emissions (which itself causes challenges with nearby electronics), be susceptible to the skin effect, become more susceptible to reflections, and even capacitively couple with other nearby traces more easily. Therefore, impedance control is an essential task for engineers when designing high-speed signal paths so that signal integrity is maximized and losses are minimized. When operating at such high speeds, engineers should take note of every UNDERSTANDING COMMON CHALLENGES TO ROUTING HIGH-SPEED SIGNALS The most common way to improve signal integrity is to upgrade your PCB materials, but, failing this, CDRs and retimers can be used. However, these solutions are often expensive and difficult to integrate, which is where Samtec Flyover ® systems become beneficial." 9 Samtec Flyover ® Solutions Break Next-Gen System Architecture Constraints

Articles in this issue

Links on this page

view archives of Supplier eBooks - Samtec - Flyover ® Solutions Break Next-Gen System Architecture Constraints