Supplier eBooks

TE Connectivity - Advancements in Industrial Automation: Smart Manufacturing and Future Technologies

Issue link: https://resources.mouser.com/i/1529320

Contents of this Issue

Navigation

Page 30 of 41

mouser.com/te 31 Comparison of Network Topologies/ Power Distribution Structures PoDL supports only point-to-point connections. IEEE 802.3da investigations are ongoing to extend PoDL to power several PDs with one PSE. Here, the focus is on data rates of 10Mbps only. By splitting signal and power onto separate lines using the hybrid cabling solution, we obtain more freedom in implementing the power network. With the additional power lines of the hybrid connector, more than one PD can be powered, and, alternatively, PoDL can be used simultaneously. Figure 5 shows examples of possible topologies to power devices (represented by nodes) in a network. Figure 5: Network topologies hybrid connector: (a) Point to point, (b) SPE daisy chained and power on a bus, (c) switch with a hybrid power source, (d) SPE and power on a bus. (Source: TE Connectivity) • Point-to-point (P2P) cabling solution (a): This is similar to most Ethernet communication. Here, the power over the separate power lines is applied point-to-point in case we need to have a high amount of power for one PD. In case PoDL is used in addition, we can use the power lines to power devices like actuators that generate electromagnetic compatibility (EMC) noise and supply power to noise-sensitive devices like the SPE PHY chips with PoDL. • SPE daisy chained and power on a bus (b): In automation networks, the devices are often installed in a daisy chain topology where every device contains a network switch. With the M12 hybrid connectivity solution, the power can be supplied directly to all devices via one power source. • Hybrid SPE switching solution (c): From a switch with a hybrid power source, the power to multiple devices can be delivered via one power source. • SPE and power on a bus (d): Multidrop SPE does not have the possibility to add PoDL. With the hybrid solution, the power can be supplied via the extra power lines. PoDL supports only point-to-point connections. " "

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - Advancements in Industrial Automation: Smart Manufacturing and Future Technologies