Supplier eBooks

Analog Devices - 14 Experts Discuss Motor Control in Modern Applications

Issue link: https://resources.mouser.com/i/1530688

Contents of this Issue

Navigation

Page 8 of 26

Every motor requires some sort of current sensing if you want to control it efficiently. Position sensing can add precision, but it's often a balance between cost and necessity, depending on the application." C h a p t e r 1 | M o t o r T y p e s a n d T h e i r C o n t r o l C h a l l e n g e s industrial robots. However, BLDC motors are more complex to control than their brushed counterparts. Control of a BLDC motor typically involves electronic commutation, in which the motor's windings are switched in a specific sequence based on the rotor's position. The most prevalent types of control are block commutation and FOC/vector control. Sensor-based control is essential for precise and reliable torque, velocity, and position control. There is a variety of position sensors (encoders) that can be used depending on the application requirements. The resolution of the encoder, the quality of the current measurement, and the implementation of the controller structure define the quality of the motor control. A sensor-based system is mandatory for position control systems as it is in robotics. Sensorless control is particularly challenging at low speeds, at which the back EMF is too weak to provide accurate feedback. This shortcoming makes low-speed control difficult in sensorless systems, especially in high-torque applications. For example, in industrial robots or drones, BLDC motors must operate across various speeds and torques. Therefore, Derrick Hartmann Senior Manager, System Architecture, Analog Devices 9 14 Experts Discuss Motor Control in Modern Applications

Articles in this issue

Links on this page

view archives of Supplier eBooks - Analog Devices - 14 Experts Discuss Motor Control in Modern Applications