Supplier eBooks

TE Connectivity - 7 Experts on Design Considerations for Fleet Telematics

Issue link: https://resources.mouser.com/i/1490533

Contents of this Issue

Navigation

Page 6 of 24

complete protection against dust over an extended time and is protected against short periods of immersion in water at depths between 15 cm and 1 m. Designing to meet such standards is a meticulous process encompassing everything from the design of the physical enclosure to the materials used within the system. Consider a key fleet telematic component like the antenna. Designing the antenna's enclosure to be sealed off from water and selecting materials that can withstand high temperatures may be important depending on the use case. However, the cost is often a design tradeoff, as rugged materials are generally more expensive. While reliability is important, if the bill of materials (BOM) for a system is cost prohibitive, then the design is not feasible. TE Connectivity helps its customers design environment-resistant fleet telematics systems by: • Leveraging a long-standing history of working on ruggedized electronics, such as external and outdoor antennas. • Offering the support necessary to help customers understand their requirements and choose the correct components. • Assisting in the design and system integration necessary for meeting standards such as IP67. C h a p t e r 1 | E n v i r o n m e n t a l D e s i g n C o n s i d e r a t i o n s Dr. Jane Yun Antenna Solutions Architect, TE Connectivity Meeting environmental standards comes down to the design and choice of the material in the BOM. However, the product must go through a series of tests to ensure that all the required specifications in all the required environmental conditions are met." 7 7 Experts on Design Considerations for Fleet Telematics

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - 7 Experts on Design Considerations for Fleet Telematics