Supplier eBooks

TE Connectivity - 7 Experts on Design Considerations for Fleet Telematics

Issue link: https://resources.mouser.com/i/1490533

Contents of this Issue

Navigation

Page 5 of 24

C h a p t e r 1 One of the primary design considerations for fleet telematics is the environmental conditions in which systems must operate. For example, in a fleet of delivery vehicles, the same asset may be expected to operate in a variety of conditions, including heat, cold, rain, and snow. Because the real value proposition of fleet telematics is the ability to constantly and reliably track an asset, maintaining the reliable operation of the asset, regardless of conditions, is particularly important. Hence, if the asset is expected to perform reliably in a variety of conditions, so too must the fleet telematics. From a hardware perspective, the major external variables to consider are temperature, moisture, and dust, all of which can be detrimental to an electronic system's performance. Beyond the external environment, the internal environment of an asset may also be an important design consideration. For example, sensors that monitor the performance of a vehicle's engine must be designed to withstand heat, dust, moisture, vibration, and electrical noise. To design ruggedized electronics capable of withstanding harsh conditions, several standards must be met. One important standard for designers to strive for is IP67, which indicates that the device has ENVIRONMENTAL DESIGN CONSIDERATIONS Darius MaliĊĦauskas Head of Electronics and Mechanical Engineers, Teltonika Telematics If you want to have a sustainable business - you have to have a sustainable environment and help foster it. You have to take into consideration the full lifecycle of the product, the materials that go into it, and even the packaging. With clever engineering, everything is possible." 6 7 Experts on Design Considerations for Fleet Telematics

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - 7 Experts on Design Considerations for Fleet Telematics