Supplier eBooks

TE Connectivity - 7 Experts on Design Considerations for Fleet Telematics

Issue link: https://resources.mouser.com/i/1490533

Contents of this Issue

Navigation

Page 12 of 24

C h a p t e r 3 As aforementioned, the design of a fleet telematics system will largely be influenced by the specific application. While the examples so far have related to vehicles, in practice, fleet telematics can track other assets, including packages and construction and industrial equipment. Because of this wide variety of applications, no two fleet telematics solutions will ever be identical and each solution will come with unique design challenges. For example, consider how the design of a system for a fleet of construction equipment may differ from that for a fleet of automobiles. A marine deployment will generally require systems that can withstand wet conditions and support longer-range connectivity in remote areas. Such considerations greatly influence fleet telematics design. Applications can also influence the design through the way that different components may need to be integrated. For example, the behavior of an antenna changes based on the surface it is mounted to. An antenna mounted on a metal surface behaves very differently than an antenna mounted on a plastic or fiberglass surface. Hence, if the application calls for a metal chassis and an external antenna, the antenna design will require special considerations. By understanding the application, designers can design antennas accordingly to ensure high performance. APPLICATION DESIGN CONSIDERATIONS The system design plays a vital role in selecting any Fleet Management Systems. The clients want an informative application design that can deliver them all the necessary information in one glance in an understandable format." Mohammed Ibrahim Field Application Engineer, Ruptela 13 7 Experts on Design Considerations for Fleet Telematics

Articles in this issue

Links on this page

view archives of Supplier eBooks - TE Connectivity - 7 Experts on Design Considerations for Fleet Telematics