Supplier eBooks

ADI - Powering the Future: Advanced Power Solutions for Efficiency and Robustness

Issue link: https://resources.mouser.com/i/1527303

Contents of this Issue

Navigation

Page 7 of 29

Another challenge is current collapse with aluminum GaN (AlGaN) and GaN HEMT devices. For these devices, a high bias voltage at the drain can result in leakage current degradation, which may be caused by carrier traps. Moreover, the two-dimensional electron gas (2DEG) concentration in the AlGaN or GaN conductive channel decreases due to a change in polarization charge generated by the surface state/effect, resulting in current collapse. Lastly, even a slight disturbance in the energy band structure boundary and material structure of ALGaN or GaN may cause 2DEG collapse. With proper device and circuit design, engineers can overcome these challenges and realize the full potential of GaN devices. Meeting those requirements, Analog Devices LTC7890/LTC7891 synchronous step-down controllers for GaN FETs include many features that mitigate the challenges of working with GaN FETs in power device design. Specifically, these DC-DC switching regulators ensure overcharging prevention of high-side driver supplies (Figure 1) while removing the need for catch, clamp, or bootstrap diodes. The controllers include smart near-zero dead times and resistor-enabled dead times, internal optimization, and internal smart bootstrap switches. Figure 1: A synchronous step-down controller using GaN FETs features internal optimization and smart near-zero dead times for high-efficiency operation at high frequencies. (Source: Analog Devices) Challenges However, the benefits of leveraging GaN technologies come at the cost of more complex driver electronics. Some nuances to GaN device behavior must be accounted for to achieve optimum performance and prevent early device failures. To achieve the higher switching speed capability of GaN devices, designers must also employ faster and more precise control systems and electronics. 8 ADI | Powering the Future

Articles in this issue

Links on this page

view archives of Supplier eBooks - ADI - Powering the Future: Advanced Power Solutions for Efficiency and Robustness