Supplier eBooks

ADI - Powering the Future: Advanced Power Solutions for Efficiency and Robustness

Issue link: https://resources.mouser.com/i/1527303

Contents of this Issue

Navigation

Page 21 of 29

Generating Negative Voltages— Why You Need Level Shifting in Buck-Boost Circuits By Frederik Dostal, Field Applications Engineer, Analog Devices, Inc. Introduction The magnitude of the negative voltage generated by inverting buck-boost circuits can be higher or lower than that of the available positive voltage. For example, −8 V or even −14 V can be generated from +12 V. When working with a switching regulator IC with an inverting buck-boost circuit, communications pins may be needed in the system design. If they are, it is essential for designers to remember adequate level shifting so that synchronization and enable signals can be utilized. Adobe Stock / Kampan – stock.adobe.com What to Consider When Designing Level Shift Circuits The inverting buck-boost topology is one of the basic switching regulator topologies, requiring just one inductor, two capacitors, and two MOSFETs as switches. The switches can be driven with any buck regulator or controller, so the availability of possible switching regulator building blocks is large. Figure 1 shows the inverting topology with all the necessary components. Figure 1: An inverting buck-boost topology for generating a negative voltage with a step-down (buck) switching regulator. (Source: Analog Devices) 22 ADI | Powering the Future

Articles in this issue

Links on this page

view archives of Supplier eBooks - ADI - Powering the Future: Advanced Power Solutions for Efficiency and Robustness