Supplier eBooks

ADI - Powering the Future: Advanced Power Solutions for Efficiency and Robustness

Issue link: https://resources.mouser.com/i/1527303

Contents of this Issue

Navigation

Page 24 of 29

Parasitic Oscillation in Hot Swaps By Aaron Shapiro, Product Applications Engineer, Analog Devices, Inc. Introduction Hot swap, surge stopper, eFuse, and ideal diode controllers that use high-side N-channel MOSFETs (NFETs) can suffer from oscillation during startup and voltage/current regulation. Datasheets typically mention this issue briefly, along with the recommended fix of adding a small gate resistor. However, without a clear understanding of the root cause of oscillations, designers may position the gate resistor poorly in the layout, making the circuit susceptible to oscillation. This article will discuss the theory behind parasitic oscillation and may prevent a board revision. Initially, adding gate resistance may seem redundant, as the resistance looking into the NFET's gate is infinite. Users may omit the part with no consequence and question whether the gate resistor was necessary. However, the 10Ω gate resistor serves as a preventative measure to suppress ringing on the gate node. The gate node possesses the components of a tank circuit, starting from the gate trace itself. A long PCB trace introduces parasitic inductance and distributed capacitance to a nearby ground plane, creating a high-frequency path to the ground. Power FETs that are optimized for a high safe operating area (SOA) have nanofarads of gate capacitance, which is further exacerbated when additional FETs are connected in parallel for increased current handling. Zener diodes used to clamp a FET's V GS also contribute parasitic capacitance (although C ISS from a power FET dominates). Figure 1 shows a generic PowerPath™ controller with parasitics drawn in. When the circuit is rotated (Figure 2), its resemblance to a Colpitts oscillator becomes evident (Figure 3). It's a tank circuit with added gain, capable of generating sustained oscillations. This configuration is found in PowerPath controllers that utilize N-channel FETs. Figure 1: A generic PowerPath controller. (Source: Analog Devices) Figure 2: A rotated PowerPath controller. (Source: Analog Devices) Figure 3: A Colpitts oscillator. (Source: Analog Devices) Adobe Stock / luchschenF – stock.adobe.com 25 Advanced Power Solutions for Efficiency and Robustness | ADI

Articles in this issue

Links on this page

view archives of Supplier eBooks - ADI - Powering the Future: Advanced Power Solutions for Efficiency and Robustness