Supplier eBooks

ADI - Powering the Future: Advanced Power Solutions for Efficiency and Robustness

Issue link: https://resources.mouser.com/i/1527303

Contents of this Issue

Navigation

Page 10 of 29

For power converters, a hot loop PCB layout with minimum parasitic parameters can improve the power efficiency, lower the voltage ringing, and reduce EMI. " " Hot Loop PCB ESR and ESL vs. Decoupling Capacitor Position In this section, the impacts of C IN position are investigated based on Analog Devices' DC2665A-B demo board for the LTM4638 µModule ® regulator. The LTM4638 is an integrated 20V IN , 15A step-down buck converter module in a tiny 6.25mm × 6.25mm × 5.02mm BGA package. It offers high power density, fast transient response, and high efficiency. The module integrates a small HF ceramic C IN inside, though it is not sufficient yet, limited by the module package size. Figures 2 through 4 illustrate three different hot loops on the demo board with additional external C IN . The first one is the vertical hot loop 1 (Figure 2), where C IN1 is placed on the bottom layer just beneath the μModule regulator. The µModule V IN and GND BGA pins are connected to C IN1 directly through the vias. These connections provide the shortest hot loop path on the demo board. The second hot loop is the vertical hot loop 2 (Figure 3), where C IN2 is still placed on the bottom layer but moved to the side area of the μModule regulator. As a result, an extra PCB trace is added to the hot loop, and larger ESL and ESR are expected compared to vertical hot loop 1. The third hot loop option is the horizontal hot loop (Figure 4), where C IN3 is placed on the top layer close to the μModule regulator. The µModule V IN and GND pins are connected to C IN3 through the top layer of copper without going through vias. Nevertheless, the V IN copper width on the top layer is limited by the other pinout, resulting in an increased loop impedance compared to that of vertical hot loop 1. Figure 2: Vertical hot loop 1: (a) top view and (b) side view. (Source: Analog Devices) Figure 3: Vertical hot loop 2: (a) top view and (b) side view. (Source: Analog Devices) Figure 4: Horizontal hot loop: (a) top view and (b) side view. (Source: Analog Devices) Adobe Stock / Hseyin – stock.adobe.com 11 Advanced Power Solutions for Efficiency and Robustness | ADI

Articles in this issue

Links on this page

view archives of Supplier eBooks - ADI - Powering the Future: Advanced Power Solutions for Efficiency and Robustness