Supplier eBooks

Microchip - Silicon Carbide Power Solutions

Issue link: https://resources.mouser.com/i/1518066

Contents of this Issue

Navigation

Page 10 of 27

Naveed ur Rehman Malik Motor Drives Engineer, Dyson C h a p t e r 2 One of the biggest challenges faced with SiC devices is their higher cost relative to Si devices, often giving the impression that SiC designs are more expensive. However, considering the benefits that SiC can bring to high- power applications, SiC can reduce not only design costs (through reduction in the size of passive components, operation at higher temperature, and removal of redundant parts) but also development costs when SiC is used in conjunction with Microchip's SiC digital gate drivers and development kits (see Chapter 3 – SiC Speed to Market). The first factor making Microchip's SiC the lowest system cost is the unrivalled ruggedness and performance provided by Microchip's SiC devices. Microchip's SiC metal–oxide–semiconductor field-effect transistors (MOSFETs) have a lower increase in R DS(on) as the temperature increases, meaning fewer devices are needed in parallel to meet power system requirements. Additionally, SiC devices have a positive LOWERING SYSTEM COST WITH SiC As SiC can withstand higher temperatures, the reliability and lifetime of the device is far greater compared to Si which in turn will reduce the cost in the long run use. As SiC devices can withstand higher temperatures, smaller and lighter cooling systems can be used resulting in considerable cost savings." 11 Silicon Carbide Power Solutions

Articles in this issue

Links on this page

view archives of Supplier eBooks - Microchip - Silicon Carbide Power Solutions