5 Practical Ways AI Strengthens Cybersecurity

(Source: Steven/stock.adobe.com; generated with AI)
Published April 22, 2026
The glut of data from new sources, combined with new ways of working with data, is making cybersecurity more complicated. But artificial intelligence (AI) delivers smarter strategies by considering context at scale.
It’s not news that enterprises are processing large amounts of data. However, the number of data sources and their associated attack surfaces are increasing. The growth of agentic AI and autonomous bots, the Industrial Internet of Things (IIoT), generative AI, and associated large language models (LLMs) is creating more opportunities for threat actors to sneak in and more complex network architectures that organizations must monitor.
While threat actors might use AI to launch cyberattacks, enterprises can, in turn, rely on the same technology to enhance their cyber hygiene. The cybersecurity field itself is evolving, harnessing the potential of AI at scale.
In this blog, we discuss five strategies AI can use to boost cybersecurity. These strategies include:
- executing strategies across distributed environments
- overcoming the limitations of static signatures
- automating gatekeeping actions in context
- ranking and prioritizing exposure and vulnerability management
- understanding threat actor psychology
Executing Strategies Across Distributed Environments
Cybersecurity must account for how and where data move, both on premises and in the cloud. And those data need protection, whether static or in transit. A Zero Trust framework, which ensures that every access request is verified, helps. In addition, role-based access control (RBAC) ensures intelligent access to sensitive data.
AI carries out these tactics at scale. The technology is also adept in IIoT environments, where attacks can take the form of unauthorized command execution instead of more familiar methods like malware infections. AI helps execute cybersecurity in today’s highly distributed data environments. Whether data management involves an understanding of telemetry, network traffic, and machine states, AI can be trained on what “normal” looks like and catch deviations from the norm, and in the right context.
For example, AI agents can be trained to guard specific categories of attack surfaces, while proprietary machine learning (ML) models can be trained to recognize threats that are unique to the enterprise workflow.
As part of AI defenses, teams can automate early actions, such as isolating breach environments or restricting network access, to limit the damage from a cyberbreach.
Overcoming the Limitations of Static Signatures
A battle-tested cybersecurity strategy is to maintain a catalog of past threat actors and match new attacks against established “signatures,” such as their IP address. Such signature-based detection should comprise one aspect of security, but not the sole one. Threat actors can change signatures very quickly, and the method doesn’t factor in zero-day exploits from entirely new sources.
Drift-aware AI models can track changes to the network environment, including cloud autoscaling and remote work, to continuously update internal records of potential new attack surfaces that need monitoring. ML models group events based on behavioral similarity rather than static, unchanging signatures, which can quickly become outdated. Equally important, these mechanisms can withstand the onslaught of data from hundreds of thousands, if not millions, of distributed nodes.
Automating Gatekeeping Actions in Context
Because some of the most complex infrastructures integrate information technology (IT) and operational technology (OT), AI models analyze how devices communicate and respond to commands. If command sequences deviate from normal established patterns, AI flags the activity as suspicious. These actions and the continuous flow of threat updates from security information and event management (SIEM), endpoint detection and response (EDR), network detection and response (NDR), and software-as-a-service (SaaS) logs might give us the picture; but acting on every alert is probably not warranted, and is the reason why cybersecurity teams need information about threat context.
Contextual enrichment models enhance data with additional relevant information that could improve understanding of the event. In this context, AI models can assign probabilistic risk scores rather than simpler binary yes-or-no models for threats. Additionally, a cybersecurity strategy should acknowledge that assigned risks can increase over time.
Ranking and Prioritizing Exposure and Vulnerability Management
Enterprises have hundreds of thousands of common vulnerabilities and exposures (CVEs), and with constantly changing inventories, they have limited capacity to keep up with all evolving threats.
AI-driven predictive analytics help cybersecurity teams understand which vulnerabilities are more likely to be exploited. In addition, the technology identifies the most likely attack paths and identities. All of these attack surfaces have to be taken together in context. For example, a CVE in an isolated system out in the field might have an overall lower vulnerability profile than a user with high privilege-identity access using a commercial browser for routine work.
Understanding Threat Actor Psychology
Cybersecurity teams can also employ psychological operations (psyops), which involve understanding and influencing an “enemy’s” mind. AI can boost cyberpsychology-informed security by exploiting an attacker’s cognitive weaknesses. For example, the attacker might have seeded innate biases that can help guide the next step in a cyber-defense system.
While such a system might not keep threat actors away forever, it can thwart or delay an attack long enough for more severe defense measures to take effect. For now, this advanced method works primarily for human-driven cyberattacks—not AI bots—but it’s a fast-evolving field of study to accommodate the next generation of AI threat actors.
Conclusion
While cyber attackers are deploying increasingly sophisticated AI bots, AI itself is a potent tool for keeping up with cybersecurity defenses at scale and in the right context. Equally important, AI adapts to how and where data move, so it can keep pace with how enterprise workflows operate today and into the future.