Skip to main content

How Microgrids Could Reshape Our Power Systems

Aerial image of homes and or buildings with solar panels (Source: Gaseesky Stock/ stock.adobe.com)

Smart grid technologies offer incredible potential for maintaining and improving the reliability and efficiency of the power grid. These innovative technologies achieve this by using real-time data to balance the flow of electricity while managing supply and demand. However, this isn't always feasible in remote areas or regions with fluctuating renewable power sources. Communities in the mountains, for example, face several unique challenges when it comes to power supply. Existing power grids in these locations are often underdeveloped and it’s expensive to install and maintain infrastructure on steep slopes, not to mention that these areas are prone to severe weather and temperature fluctuations. This is where microgrids come into play. These localized power systems can directly integrate renewable energy sources, offering greater flexibility and resilience in areas with limited grid access or unreliable central power.
In this blog, we’ll explore how microgrids fit within the landscape of smart grid technologies, as well as consider their ability to reshape our power systems, integrate renewable energy sources, and pave the way for a more sustainable future. Lastly, we’ll discuss the path forward for widespread adoption of these innovative solutions.

The Limitations of Traditional Power Grids


Traditional large-scale power grids with centralized structures face limitations in an evolving energy ecosystem. These systems rely on one-way power flow, typically from fossil fuel or nuclear sources, transmitted over long distances through high-voltage lines. While effective in delivering electricity, they lack the flexibility and efficiency needed for a sustainable future. Limited communication capabilities hinder real-time monitoring and optimization, while the absence of energy storage creates challenges with integrating renewable sources with fluctuating generation patterns. Additionally, traditional grids operate solely based on demand, offering little control over consumption patterns and the potential for peak overloads.


Smart Grids Answer the Call


Smart grids offer the potential to revolutionize power supply by transforming the one-way flow of traditional grids. They leverage a network of smart meters, sensors, control systems, and two-way communication to gather real-time data on electricity usage and grid conditions. Advanced algorithms analyze this data to optimize energy use, minimize waste, and predict demand fluctuations. Unlike their predecessors, smart grids can seamlessly integrate renewable energy sources like solar and wind, paving the way for a more sustainable and reliable energy system.


Microgrids as Localized Power Systems


Smart grids represent a significant leap forward in managing large-scale energy systems. However, their vast reach can present challenges in terms of complexity and cost, especially for geographically dispersed areas. Additionally, integrating renewable energy sources with variable output can disrupt the delicate balance of supply and demand across extensive grids, requiring additional infrastructure upgrades to ensure stable energy flow.


Microgrids offer a compelling solution, promoting a more decentralized energy generation and supply approach. Unlike sprawling smart grids, microgrids are self-contained power systems operating locally. The localized grouping of electricity sources and loads can either connect to the traditional centralized electrical grid (macrogrid) or disconnect to “island mode” and function autonomously. This localized structure makes them well-suited for powering remote communities and enabling them to achieve energy independence, efficiency, and reliability. In addition, by generating power closer to where it’s consumed, microgrids reduce energy loss that occurs during transmission and distribution over long distances. Microgrids can incorporate various sources of energy generation, including renewables like solar and wind, combined heat and power (CHP) systems, batteries, and other forms of energy storage. This mixture allows them to provide power during outages on the main grid, improve energy efficiency, and even reduce costs. 


Primary Locations for Microgrids
Microgrids can be found in a variety of settings, ranging from industrial complexes, military bases, and university campuses to rural communities and remote locations. They’re particularly valuable in areas where the main grid is unreliable or where there’s a high demand for energy security and quality. For remote or isolated communities, microgrids offer a path to energy independence and economic development, reducing or eliminating the need to rely on expensive and often less reliable energy imports. Moreover, in areas without existing grid infrastructure, microgrids represent a viable and cost-effective solution for electrification, providing access to electricity that can support education, healthcare, and local economic activities. 

Another key use case for microgrids is backup power for critical infrastructure. Hospitals, police stations, and airports require uninterrupted power for essential services. Microgrids can act as reliable backup power sources, being equipped with batteries or generators that seamlessly kick in during a grid outage to ensure critical facilities remain operational even when the main grid fails.

Microgrids to Leverage Renewable Energy
Renewable energy sources offer a clean and sustainable future, but their dependence on weather can cause fluctuations. Wind farms need backup during calm periods, as do solar panels when there isn't enough sun. Battery energy storage systems (BESS) can bridge this gap. These systems capture excess power generated during peak wind or sunshine hours and store it for use during low-production periods. Microgrids can leverage BESS to store renewable sources like solar, wind, and tidal. This approach strengthens grid resilience by providing a more reliable source of clean energy and reducing strain on the main grid, especially during peak demand periods. In addition, these battery systems can enable microgrids to operate autonomously during outages on the main grid and help ensure the continuity of critical services even during widespread blackouts.


What makes microgrids even more promising is that they can be put in the right place to harness these different energy types and then use that energy locally to optimize efficiency. Take, for example, putting another 3,000 houses on a mountain. Extending power lines, building substations uphill, and deciding which existing substations can take the load is costly and time-consuming. Microgrids, meanwhile, are a lot smarter, acting like miniature grids to generate power locally and manage it within the community. They enable enhanced monitoring and control with remote terminal units (RTUs) and supervisory control and data acquisition (SCADA) systems while offering improved security thanks to the localized control. Since microgrids can operate autonomously, they are less reliant on the main grid and potential risks are minimized. Still, the technology and operational strategies behind microgrids are complex, involving advanced power electronics, control systems, and energy management solutions to ensure that power generation is optimized and resources are used efficiently, whether in connected or island mode.


Embracing the Power of Solar Shingles
Microgrids also offer an exciting opportunity to harness innovative solutions like solar shingles. The real estate is already there, so it's not a case of needing the infrastructure or finding the space for large solar farms. Widespread adoption of microgrids would hold immense potential for achieving sustainable power, transforming rooftops into miniature power plants without the added infrastructure development for solar panels. Currently, there's growing interest in community microgrids. Some existing examples involve neighborhoods or apartment complexes collaborating on solar installations and energy sharing. Microgrids can help reduce electricity costs through more efficient energy use and by allowing consumers to generate their own power, reducing the need to purchase electricity from the grid. Every new house built with solar shingles could create more community microgrids, share excess energy, increase resilience, and create a more autonomous power system. 


Challenges Facing Wider Microgrid Adoption


The road to a sustainable energy future has its challenges. Red tape often prevents energy from being passed up or down the grid as required, and existing infrastructure can create hurdles to the widespread adoption of renewable energy sources. However, innovative solutions like microgrids offer an exciting opportunity to create a more efficient and adaptable energy ecosystem. 


Microgrids empower communities to harness clean energy, reducing reliance on traditional grids and fostering energy independence. Their ability to store excess energy locally minimizes dependence on external sources and mitigates the limitations of current grid infrastructure. Nevertheless, we might be underutilizing microgrids by only focusing on their essential features. These localized systems hold immense potential for advanced energy management, including intelligent load balancing, real-time optimization of renewable energy sources, and seamless integration with energy storage solutions. So, while their potential is undeniable, regulatory frameworks certainly need considerable adjustments. 


The Future of Sustainable Power Supply


Looking ahead, microgrids can serve as building blocks for a more distributed and resilient energy landscape. Integrating various renewable energy sources and advanced energy management systems opens up opportunities for a cleaner and more reliable power supply, thereby supporting efforts to combat climate change. In the future, microgrids could seamlessly interact with a smarter, more responsive main grid. This interconnected ecosystem would allow for real-time balancing of energy supply and demand, further optimizing the use of renewable resources and minimizing reliance on traditional power plants. Overall, microgrids represent a versatile and forward-looking approach to energy generation and distribution, aligning closely with global goals for sustainability, resilience, and economic development. 


The opinions and views expressed in this article are solely those of the author and do not reflect or represent the author's affiliated company.

About the Author

Courtney Gross is a Solutions Engineer with over 5 years of experience specializing in telecommunication and renewable resource solutions. At AEP, she spearheads the development and implementation of cutting-edge technology solutions tailored to meet unique business challenges. An expert in cross-functional collaboration, Courtney delivers impactful customer-centric solutions, driving significant improvements in system efficiency and security. Passionate about innovation, she continually seeks to expand her knowledge and expertise.

Profile Photo of Courtney Gross