Skip to main content

Engineering Metamaterials That Behave Beyond Nature

The materials available to engineers have always influenced what they can build. As the electronics industry has advanced, engineers have needed to find materials that can meet the demands of new applications. Specialized dielectrics support high-frequency circuits, while ceramics, composites, and advanced alloys provide properties suited to more demanding applications and environments. In each case, engineers select materials based on the electrical, mechanical, or physical properties required for a given application. 

And while for most materials, those inherent properties set the boundaries of what an engineer can work with, metamaterials expand those boundaries by making structure part of the design. Metamaterials can be made from familiar materials, including metals, ceramics, glass, and polymers, but their behavior is dictated by the geometry and arrangement of engineered features within them. By changing those features, engineers can influence how a material interacts with electromagnetic energy or responds to mechanical forces, creating behaviors that would not typically come from the base material alone. 

One way to visualize this concept is to think of a mosaic. A single tile may have simple characteristics, but when thousands of tiles are arranged in a precise pattern, they create something that an individual tile cannot. In a metamaterial, engineered structures work together in a similar way to produce behavior that emerges from their collective arrangement. 

Early interest in metamaterials focused on controlling electromagnetic waves, but the same fundamental concept has spread to other areas of engineering: using structure to create a response that conventional materials alone cannot provide.1  Researchers are applying this concept to wireless communications, optics, radar, sensing, and mechanical systems, among other fields. In addition, advances in fabrication and computational design are making increasingly complex structures practical to manufacture. What began primarily as a research concept is now finding its way into practical engineering applications and commercial devices, offering designers another way to resolve problems that are too difficult to solve through simple material selection.2

This article explores how metamaterials use engineered structures to create properties that conventional materials cannot achieve. It also examines emerging applications across wireless communications, optics, sensing, and mechanical systems, as well as the advances in design and fabrication that are enabling their adoption.

How Metamaterials Work


Although the term might sound like it refers to a completely new class of materials, metamaterials can be made from many conventional materials, such as aluminum, glass, ceramic, silicon, and polymers. What distinguishes them is the engineered structure that works with the base material’s properties to produce a behavior.3 

Many metamaterials are built from structural elements called unit cells. These small structures are arranged in designed patterns throughout the material. Engineers can tailor the resulting material’s overall response to electromagnetic energy or mechanical forces by controlling its geometry, spacing, orientation, and dimensions.  

The structures used in electromagnetic metamaterials are typically smaller than the wavelength they are designed to control. The waves, therefore, respond to the collective properties of the patterned structure.

The resulting material’s overall properties depend not only on what it is made from but also on how the small structures are designed and arranged, often described as the material’s effective properties.4  By changing the structure, engineers have another way to control how the material behaves without changing the base material itself.5

Engineering New Material Behaviors


Depending on the design, metamaterials can influence wave propagation, reflection, transmission, absorption, and phase. The ability to engineer material behavior rather than select it opens new engineering possibilities across many fields, including wireless communications, optical systems, radar, and sensing. Although the underlying physics may differ, the basic idea remains the same. 

Smaller and More Flexible Wireless Systems

One of the more mature applications of metamaterials is in antenna design. Wireless devices continue to shrink while supporting more frequency bands and higher data rates. This creates challenges for antennas, whose performance is closely tied to physical size. Engineered metamaterial surfaces offer a way to reduce antenna size while maintaining, or even improving, performance.6

However, metamaterial antennas should not be confused with electrically small antennas (ESAs). ESAs are an established class of antennas defined by their size relative to the operating wavelength, whereas metamaterial antennas are defined by the use of engineered structures or materials to influence electromagnetic behavior. These concepts sometimes overlap because metamaterial techniques can miniaturize an antenna, but the terms do not refer to the same thing.

For example, satellite communications company Kymeta has commercialized flat-panel satellite antennas that use a metasurface to electronically steer the antenna beam, eliminating the need to point a conventional satellite dish mechanically.7  This enables satellite connectivity to be integrated into a thin, low-profile antenna that works on mobile platforms.

Reimagining Optical Systems

The same principles apply to visible and infrared light. One area of interest is the development of flat lenses, also called metalenses, which use microscopic structures patterned on a thin surface to control light rather than relying on the shape of a traditional curved lens.8

One technology where this can be impactful is light detection and ranging (LIDAR). Conventional lidar systems rely on optical components to direct and focus light, which adds size and complexity to the sensor. Researchers have demonstrated lidar beam-steering systems that incorporate a metalens to control the output beam while reducing the size of the optical system, creating a more compact structure that is easier to integrate and assemble.9  Metalenses are also being explored for microscopy, medical imaging, and other sensing applications.


Improving Radar and Electromagnetic Control

Radar and sensing systems can also benefit from greater control over electromagnetic waves. Automotive radar, industrial sensors, and aerospace systems all depend on accurately transmitting and receiving electromagnetic signals.

In automotive applications, radar sensors often must fit within compact vehicle designs while detecting relatively weak reflected signals. Metamaterials can give engineers another way to shape and direct the radar beam within those space constraints.

Engineers can also design metamaterial structures to direct, absorb, or filter electromagnetic energy for applications such as absorbers, shielding, and waveguides. This enables better management of interference, signal propagation, and electromagnetic behavior in increasingly compact systems.

Mechanical Metamaterials


While metamaterials are garnering significant attention for their electromagnetic properties, the same design concept can be applied to mechanical systems. Rather than controlling electromagnetic waves, mechanical metamaterials use engineered internal geometries to control how a material responds to mechanical forces.

Through tailored internal architecture, these materials can exhibit counterintuitive properties, such as auxetic behavior. Unlike most materials, which thin when stretched, auxetic materials expand laterally. This behavior, known as a negative Poisson’s ratio, can enhance impact resistance and energy absorption.10

Mechanical metamaterials are being explored for applications including athletic helmets, robotics, medical implants, and aerospace structures.

Technologies Driving Metamaterial Adoption


Metamaterials are not a new concept, but advances in manufacturing and design tools have made it increasingly feasible to create these complex structures. Additive manufacturing has been important in this area because it enables engineers to fabricate intricate geometries that would be difficult or even impossible to produce using methods such as machining, molding, or standard lithography techniques.11 

Semiconductor fabrication has also enabled the creation of small, repeatable structures, and advances in simulation and computational optimization have allowed engineers to test various geometries and evaluate their performance before building a physical prototype.12

Artificial intelligence (AI) and machine learning (ML) are beginning to help researchers explore larger design spaces and identify potential structures more efficiently.13  These advances are making metamaterials more practical to design and manufacture, which is a key reason engineers are paying more attention to them now, as they can finally move from theoretical designs to buildable applications.

Conclusion


Metamaterials give engineers a new approach to material design. By carefully controlling internal structure and material composition, they can create electromagnetic or mechanical behavior that suits a particular application. Advances in fabrication and computational design are making these structures more practical and expanding their potential across wireless, optical, sensing, and mechanical systems.

 1https://www.nature.com/articles/s42254-018-0018-y
  2https://www.nature.com/articles/s41563-025-02217-7
  3https://people.ee.duke.edu/~drsmith/metamaterials.htm
  4https://www.nist.gov/publications/effective-material-property-extraction-metamaterial-taking-boundary-effects-account
  5https://www.nist.gov/publications/overview-theory-and-applications-metasurfaces-two-dimensional-equivalents-metamaterials
  6https://www.tandfonline.com/doi/abs/10.1080/09205071.2014.972470
  7https://www.microwavejournal.com/articles/28062-kymeta-announces-commercial-release-of-ku-band-metamaterial-antenna-and-satellite-data-service
  8https://www.sciencedirect.com/science/article/abs/pii/S0924424726003985
  9https://opg.optica.org/ao/abstract.cfm?uri=ao-64-11-2819
  10https://www.sciencedirect.com/science/article/abs/pii/S0141029622014535?via%3Dihub
  11https://www.sciencedirect.com/science/article/abs/pii/S2214860420309349
  12https://opg.optica.org/aop/abstract.cfm?uri=aop-15-4-1033
  13https://www.nature.com/articles/s43588-024-00672-x

About the Author

Bryan DeLuca is a seasoned electronics content creator with a deep passion for demystifying complex engineering concepts. Through years of hands-on experience, he has built a reputation for translating advanced electronics topics into practical, engaging content for engineers, hobbyists, and makers. Bryan produces technical articles and videos that focus on components, power electronics, additive manufacturing, and the integration of microcontrollers, LEDs, and sensors.

Profile Photo of Bryan DeLuca