Skip to main content

All-seeing AI: TensorFlow for image analysis

By Michael Parks for Mouser Electronics

Introduction

The second in a series of four projects exploring the convergence of embedded electronics and artificial intelligence (AI).

The combination of efficient, brain-like algorithms and inexpensive yet powerful microcontrollers and sensors has given rise to so-called edge computing. Edge computing promises billions of inexpensive embedded electronic systems interacting with the physical world nearly instantaneously. In addition, there’s no need to reach back to the processing horsepower of the cloud. When fully realized, edge computing represents a revolution in automation, both in scale and capability.

One such capability is the desire for these edge devices to augment the human worker by being a watchful protector that never blinks. One example: a function that turns off heavy machinery should someone place their hand in an unsafe location. In this project, we will look at how machine learning can be applied to image detection use-cases in a practical and meaningful manner.

Project Materials and Resources

In this chapter of our TensorFlow Lite for Microcontrollers series, we will focus on the SAM E54 Xplained Pro evaluation kit (Figure 1); a hardware platform for evaluating the ATSAME54P20A microcontroller.

 

Figure 1: Microchip Technology's SAM E54 Xplained Pro Development Kit is a hardware platform for evaluating the ATSAME54P20A microcontroller. (Source: Microchip Technology)

We will leverage the SAM E54 to build a device that incorporates a camera as an input device and an LED as user feedback. The goal is to toggle the LED on and off depending on whether a human is within the camera’s field of view.

Bill of Material (BOM)

You can click this Mouser project share link to access the BOM along with the current pricing. Table 1 lists the items in the BOM.

Table 1: TensorFlow Lite - Microchip Technology BOM

Quantity

Mouser P/N

Description

Notes

1

556-ATSAME54XPRO (Figure 2)

Development Boards & Kits - ARM SAM E54 XPLAINED PRO

 

1

713-114991881

OV2640 Camera

 

4

667-ERJ-2GE0R00X

0-ohm resistors, 0402 package, 1/16W

R205, R206, R207, R208

1

932-MIKROE-2295

24-pin FPC Cable

Between OV2640 and Adapter Board FPC

1

200-IDSD05D0300T

2x10 IDC Cable, 0.1" pitch, 3" length

Between SAM E54 and Adapter Board PCC

2

200-MTSW10508LD335

2x10 male header

SAM E54 PCC
Adapter Board PCC

1

798-FH12-24S-0.5SH55

Hirose 1x24 FPC

Adapter Board FPC

Resources

All source files for this project are located on Mouser’s GitHub repository. The repository is divided into three main folders:

 

Figure 2: A schematic view of the SAM E54 Xplained Pro development board. (Source: Microchip Technology)

Documentation

The Documentation folder contains graphic files of schematics (Figure 2) and other important reference materials.

Hardware

The Hardware folder contains schematics of the SAM E54 development board and the OV2640 camera. It also contains the schematic capture and printed circuit board (PCB) layout files for an adapter board to connect the FPC cable of the OV2640 camera to the 2x10 PCC connector of the SAM E54. The board layout was done in KiCAD, a free and open-source schematic capture and board layout application that can be downloaded: https://kicad-pcb.org.

Figure 3: The PCB and enclosure for camera adapter board. (Source: MB Parks)

3D Files

The 3D Files folder contains 3D renderings (.f3d, .step) of the adapter board PCB as well as the files needed to view and 3D print (.stl, .obj) a custom stand for the adapter board to keep it safe (Figure 3).

The files can be viewed for free at https://viewer.autodesk.com/.

If you would like to purchase the PCB, it is available at OSHPark.

The FPC connector and male headers that must be soldered onto the PCB are included in BOM.

Software

The Software folder contains the source code and the neural network model for the project. We will have to modify replace a few files with our custom implementation to interact with SAM E54 Xplained Pro development board and associated components (LED and camera interface). The files provided:

  • main.cc
  • main_functions.cc / .h
  • detection_responder.cc / .h
  • image_provider.cc / .h
  • driver_init.cc / .h
  • model_settings.cc / .h
  • atmel_start_pins.h
  • no_person_image_data.h
  • person_detect_model_data.h
  • person_image_data.h

More details about these files can be found in the Software section below.

Tools

This project assumes that you have access to the following tools:

  • Windows 7-based computer or newer with at least a 1.6GHz processor, 2GB RAM (another 512MB if using a virtual machine), and 6GB of available storage.
  • Internet connection
  • Soldering iron
  • Magnifying glass
  • Flush diagonal cutter
  • Needle-nose pliers
  • Digital Multimeter (DMM)

Documentation

Additional resources and documentation regarding the Xplained Pro series of development boards as well as the TensorFlow Lite for Microcontrollers Software Development Kit (SDK) are available. Some of the recommended documentation to review:

Machine Learning Technology Overview

The SAM E54 Xplained Pro Development Board (Figure 4) features a powerful ATSAME54P20A microcontroller with 32MB of Queued Serial Peripheral Interface (QSPI) Flash. The Xplained Pro development kits include an onboard Embedded Debugger to simplify programming and troubleshooting. 

 

Figure 4: Feature highlight of the SAM E54 Xplained Pro Development Boards. (Source: Microchip Technology)

Google offers several pre-trained neural network models that will work with the TensorFlow Lite for Microcontroller SDK (Figure 5).

 

 

Figure 5: Google's TensorFlow Lite for Microcontroller website has resources and pre-trained models ready for use. (Source: Google)

This project will go with the person detection example. This is an image recognition model that will leverage the development kit’s PCC connector to interface with the OV2640 camera module. The camera will provide inputs for the TensorFlow object detection model.

To deploy a TensorFlow model to a microcontroller, you will need to follow this development workflow to train Neural Network (NN) model then convert it to a format that can work on a resource-constrained device such as a microcontroller.

  • Train the Neural Network: The TensorFlow framework allows a model to be trained on a desktop computer or using the horsepower of cloud-based services such as AWS or Google Compute Engine. Bottom line: the more processing power (CPUs and GPUs) you throw at training a NN, the faster or more robust the final model will be. The result of training a model with TensorFlow is a file with a .pb extension. Downloading a pre-trained model is another option.
  • Prepare the Model for Inferencing Hardware: The next step is to take the trained model and prepare it to run on the chosen endpoint device. The model must be made small enough to fit within the memory of the SAM E54 after conversion. Additionally, the code can only use the functions that are supported by TensorFlow Lite for Microcontrollers. However, it is possible to use a function that is not currently supported if you write your own custom implementations.
    • Convert the TensorFlow model to a TensorFlow Lite FlatBuffer: You will convert your model into the standard TensorFlow Lite format using the TensorFlow Lite converter. You might wish to output a quantized model because these are smaller in size and more efficient to execute.
    • Convert the FlatBuffer to a C Byte Array: Models are kept in read-only program memory and stored in a C file. TensorFlow SDK provides tools that can be used to convert the FlatBuffer into the appropriate C byte array format.
  • Integrate the TensorFlow Lite for Microcontrollers C++ Library: Write the value-added code for our particular implementation that will allow the project to interact with the accelerometer chip to collect acceleration data, perform inferencing utilizing the TensorFlow Lite for Microcontroller C++ library, make a prediction, and then display the results to the end-user via the serial terminal.
  • Deployment to the Edge: Build and deploy the program to your device using the Atmel Studio 7 IDE.

 

Figure 6: SAM E54 board layout with required resistor modifications highlighted in red. (Source: Microchip Technology)

Putting It All Together

In this section, we will examine the necessary steps to get your project up and running. We will also point out areas where you can customize the project to meet your specific needs. This project offers some rather good opportunities to tweak the design to meet your specific needs.

The section is broken down into the following subsections:

  1. Hardware Modifications
  2. Setting up the Toolchain
  3. Software Development

Hardware Modifications

The SAM E54 contains a Parallel Capture Controller (PCC) to interact with the OV2460 camera. The physical form factor is a 2x10, 100mm pitch pin-header. By default, the PCC connector is not functional because the pins are being used by other components aboard the development board. These functions include Ethernet, QTouch, SD Card, EXT1, and EXT2. To use the PCC, we will lose the ability to use these other functions.

The good news is this project gives us the opportunity to practice two important electronics skills–desoldering and soldering surface mount components. To enable the PCC functionality, the following modifications (Figure 6) to the dev board will be required: 

  • Remove the following surface mount resistors: R621, R622, R623, R624, R625, R626, R628, R629, R630, R308
  • Insert the 2x10 male header (or two 1x10 male headers) through the top of the board and solder the pins from the bottom of the board. (Figure 7)
  • Solder 0Ω resistors to the following pads: R205, R206, R207, R208. The resistor package size is 0402 and must be rated for 1/16W at a minimum.
  • Remove any SD cards from the SD card connector

 

Figure 7: The SAM E54 development board with male headers for the camera interface now soldered on. (Source: Mouser Electronics)

 

Figure 8: PCB layout of the adapter board. (Source: MB Parks)

Next, we will solder the adapter board. It is very straightforward and requires soldering both through-hole components and surface mount components. Just solder the surface-mount FPC connector to the FPC pads. Then place the 2x10 male headers through the holes on top of the board and then solder them from the bottom of the board. The adapter board (Figure 8) lets the FPC cable of the OV2640 camera connect to the PCC connector board the SAM E54 development board. Table 2 shows the relationship of the OV2640 pins between the PCC connector and the FPC connector.

Table 2: PCC (IDC Cable) to FPC Pin Assignment Crosswalk

PCC (IDC) Pin #

Function

FPC Pin #

1

VCC

10

2

GND

15

3

SCL

5

4

SDA

3

5

VSYNC

7

6

HSYNC

9

7

PCLK

17

8

XCLK

13

9

DOUT07

16

10

DOUT06

18

11

DOUT05

20

12

DOUT04

22

13

DOUT03

21

14

DOUT02

19

15

DOUT01

23

16

DOUT00

24

17

DOUT09

12

18

DOUT08

14

19

RESET

6

20

PDWN

8

N/A

STROBE

1

N/A

AGND

2

N/A

AVDD

4

N/A

DOVDD

11

Setting up the Toolchain

There are multiple options when it comes to development environments for writing the firmware needed for this project. These options include:

  • Atmel Studio 7
  • MPLAB X IDE 5.XX

For this project, we will use Atmel Studio 7. But to begin, we will head over to Atmel’s START website (Figure 9) to grab the libraries that we need to interact with the SAM E54 development kit.

 

Figure 9: The Atmel START website allows an embedded developer to pick the libraries for their target board. (Source: Microchip Technology)

Once there, follow these steps:

  1. Click on the green button labeled Create New Project
  2. Look for the dialog box labeled Filter on Device and enter E54
  3. Select SAM E54 Xplained Pro
  4. Under Drivers place a 1 next to Camera
  5. Select Create New Project
  6. Click Export Project
  7. Ensure Atmel Studio is ticked
  8. Click Download Pack to download the .atzip file that contains the code to be imported into Atmel Studio 7.

Next, it is time to download Atmel Studio 7 (Figure 10).

 

Figure 10: Atmel Studio 7 is a convenient tool to edit your code and interact with the SAM E54 Xplained Pro development board. (Source: Microchip Technology)

Next, grab a copy of the source code from our GitHub repository. Open your command prompt, navigate to where you want to save the source code, then enter:

#git clone https://github.com/Mouser-Electronics/TensorFlow-Lite-Microchip

Once we have the software installed and libraries downloaded, we can launch Atmel Studio 7 (Figure 11).

 

Figure 11: Atmel Studio 7 when initially launched. (Source: Microchip Technology)

From the Atmel Studio 7 IDE, click file > open and then navigate to where you cloned the repository and select the project files (.cc/.h). With that, we are ready to examine the source code.

Software Development

Figure 12: Source code available on GitHub. (Source: Mouser Electronics)

The codebase for this project is written in C++. Sixteen files of interest will be found in the Software folder of the project structure of the GitHub repository (Figure 12). Files with the .h extension are the header files that contain function definition and variable declarations. The files with the .cc extension contain the logic as defined by the various classes and functions found within each source code file. The list of key files includes:

  • detection_responder.cc / .h*: These files will allow us to create a response to the user because of a person being detected in the camera’s field of view. Since the SAM E54 offers a single yellow LED that the developer can interact with, we will create a visual cue as feedback to the user. If a person is seen by the camera, we will turn on the LED. When the camera no longer sees a person, we will turn off the LED.
  • image_provider.cc / .h*: These files will allow us to interact with the OV2640 that is connected to the dev kit’s PCC. Specifically, we grab a JPEG from the camera and hand it off to the NN model to process.
  • main.cc*: This file contains the main loop that makes up this project. It is quite simple and just calls the setup() function loop once and repeatedly calls the loop() function within an endless loop.
  • main_functions.cc / .h*: Contains the setup() and loop() functions responsible for most of the high-level functionality of this project. The setup() function runs first and initializes the various data structures needed by the inferencing engine of the TensorFlow libraries. It also initializes the LED and camera hardware unique to the SAM E54. Then the loop() function takes over and it has four major responsibilities:
    • Get an image from the camera.
    • Send the image data to the neural network interpreter.
    • Receive the output from the NN which are two scores representing the likelihood that a person was in the camera’s field of view and a score representing the likelihood a person was not in the camera’s field of view.
    • Send the scores to a function to handle the LED. It does so based on the relative values of the person and no-person scores.
      You will notice that the naming convention of setup() and loop() follows that of the Arduino programming environment as the TensorFlow examples are made to compatible with various Arduino boards.
  • driver_init.cc / .h: This folder contains the code to initialize the PCC hardware on the development board so the board can interact with the OV2640 camera module.
  • model_settings.cc / .h: The folder contains variables and constants that can be tweaked to change how the model responds to inputs. The specifics of what can be changed will be discussed below.
  • atmel_start_pins.h: Contains definitions of the various GPIO pins, including the user LED, which is connected to pin PC18. Makes calling on the pins in the code much simpler and the code more portable.
  • no_person_image_data.h: Contains data that was created from a sample image without a person in it.
  • person_detect_model_data.h: Contains the TensorFlow Lite model file after being converted into a C data array
  • person_image_data.h: Contains data that was created from a sample image with a person in it.

*These files have been replaced or modified with custom written code for the SAM E54 development board to handle the OV2640 camera and GPIO pin connected to the user LED.

Key Variables and Constants

You might want to tweak a few variables depending on your particular design choices. These variables and can be found in model_settings.h and include:

  • constexpr int kNumCols = 96: Sets the number of pixel columns of the camera.
  • constexpr int kNumRows = 96: Sets the number of pixel rows of the camera.
  • constexpr int kNumChannels = 1: The number of concurrent channels (thinks streams) the camera can support.
  • constexpr int kMaxImageSize = kNumCols * kNumRows * kNumChannels: Set the total resolution of the captured image.

A note about the constant expression keyword (constexpr) that is used to define the variable a constant but does so at compile-time vs. runtime as with the const keyword.

Modified Code

Some of the files have been modified to account for the project-specific functionality we wish to add as well as tailoring for the SAM E54 development board. The following files were modified:

main_functions.cc

Adds functionality to the setup function initialize the LED and call a new function called system_init() to initialize the camera. That code is contained in driver_init.cc.

void setup() {

  

  gpio_set_pin_level(LED0, false);


 

  // Set pin direction to output

  gpio_set_pin_direction(LED0, GPIO_DIRECTION_OUT);

  gpio_set_pin_function(LED0, GPIO_PIN_FUNCTION_OFF);

  

  system_init();

  

  // Set up logging. Google style is to avoid globals or statics because of

  // lifetime uncertainty, but since this has a trivial destructor it's okay.

  // NOLINTNEXTLINE(runtime-global-variables)

  static tflite::MicroErrorReporter micro_error_reporter;

  error_reporter = µ_error_reporter;

 

  // Map the model into a usable data structure. This doesn't involve any

  // copying or parsing, it's a very lightweight operation.

  model = tflite::GetModel(g_person_detect_model_data);

  if (model->version() != TFLITE_SCHEMA_VERSION) {

    TF_LITE_REPORT_ERROR(error_reporter,

                         "Model provided is schema version %d not equal "

                         "to supported version %d.",

                         model->version(), TFLITE_SCHEMA_VERSION);

             

    return;

  }

detection_responder.cc

Adds functionality the compares the output of the neural network (person_score and no_person_score) and makes a determination to illuminate or extinguish the LED. If person_score is greater than no_person_score then the LED is lit. Otherwise, the LED is turned off.

#include "tensorflow/lite/micro/examples/person_detection/detection_responder.h"

#include

#include


 

void RespondToDetection(tflite::ErrorReporter* error_reporter,

                        uint8_t person_score, uint8_t no_person_score) {

  TF_LITE_REPORT_ERROR(error_reporter, "person score:%d no person score %d",

                       person_score, no_person_score);

  //If the NN returns a person_score that is greater than the no_person_score, turn the LED on...  

  if(person_score > no_person_score) {

  gpio_set_pin_level(LED0, true);

  }

  //...otherwise turn the LED off.

  else {

  gpio_set_pin_level(LED0, false);

  }

}

image_provider.cc

Interacts with the OV2640 camera, grabs a snapshot of the buffer, and sends it to the TensorFlow model for processing.

#include "tensorflow/lite/micro/examples/person_detection/image_provider.h"

#include "tensorflow/lite/micro/examples/person_detection/model_settings.h"

#include "driver_examples.h"

#include "driver_init.h"

#include "utils.h"

 

uint32_t frame_buf[CONF_PCC_DMA_FRAME_SIZE];

 

static void capture_cb(struct camera_async_descriptor *const descr, uint32_t ch)

{

  if (ch == 0) {

    // Application can process data in frame_buf.

    camera_async_capture_start(&CAMERA_0, 0, frame_buf);

  }

}

 

TfLiteStatus GetImage(tflite::ErrorReporter* error_reporter, int image_width,

                      int image_height, int channels, uint8_t* image_data) {

 

  camera_async_register_callback(&CAMERA_0, capture_cb);

  camera_async_enable(&CAMERA_0);

  camera_async_capture_start(&CAMERA_0, 0, frame_buf);                     

 

  for (int i = 0; i < image_width * image_height * channels; ++i) {

    image_data[i] = frame_buf[i];

  }

  return;

}

Building the Project

Launch Atmel Studio and open the necessary project files (Figure 13). The SAM E54 should be programmed and powered with the micro-USB port (debug port) that is located to the top, the right side of the development board.

Figure 13: SLayout of Atmel Studio 7 in edit mode (Source: Mouser Electronics)

Now it is time to build the project and then upload it to the development board. To accomplish this first ensure a micro-USB cable is connected between the computer and the debug port of the development board.

Figure 14: Build succeed message indicates we are ready to upload the firmware to the target device. (Source: MB Parks)

Click on Build > Build Solution. If successful, you will get a Successful Build message (Figure 14).

Next click on Debug > Start without Debugging. Since the SAM E54 has onboard EDBG hardware, ensure that EDBG is selected under Tool > Selected debugger/programmer (Figure 15). Once the project is loaded, it will automatically start running. Now that the firmware has been uploaded to the development board, let us look at the project in action.

Figure 15: Ensure that Atmel Studio 7 can see the EDBG hardware onboard the SAM E54 development board. (Source: MB Parks)

Project in Action

Figure 16: Connect the camera and power the development board with a micro-USB cable plugged into the debug USB port on the top of the board. (Source: Mouser Electronics)

With the camera and the micro-USB cable board plugged into the SAM E54 development board, let us power up the development board (Figure 16). Note, the USB cable does not have to be plugged into a computer. It can also be plugged into a USB power adapter.

Ensure that the camera is not facing a person when initially powered on. Wait for about 10 seconds and then aim the camera at a person. After a few seconds, the user LED will illuminate. Turn the camera away, and after a few seconds the LED will turn off.

While this is a simple example, toggling an LED on and off, it does provide a great starting point for more complex use cases. As mentioned, we discussed how computer vision AI could be useful in safety applications. Hopefully, it is easy to see that instead of an LED, that the GPIO could instead trigger a relay to break the current flow to heavy machinery should a person enter a location they are not supposed to be. Or a security device could sound an alert should a person be detected after hours. In short, technology will never replace humans in the realms of safety and security; but technology can help augment our eyes and ears in achieving a more safe, secure world.

About the Author

Michael Parks, P.E. is the owner of Green Shoe Garage, a custom electronics design studio and technology consultancy located in Southern Maryland. He produces the S.T.E.A.M. Power podcast to help raise public awareness of technical and scientific matters. Michael is also a licensed Professional Engineer in the state of Maryland and holds a Master’s degree in systems engineering from Johns Hopkins University.

Profile Photo of Mike Parks