Skip to main content

The Switch to 400G Ethernet

Making the Change to 400 Gigabit Ethernet

Image Source: Adobe Stock/vladmircaribb

By David Pike for Mouser Electronics

Published February 17, 2023

We live in a connected world where communication devices form a global network. We share and consume data freely and rely on telecommunications infrastructure to deliver the performance needed by the latest generation of equipment.

The ever-increasing appetite for data communications drives the need for far greater capabilities. The Internet of Things (IoT), advances in artificial intelligence (AI) and machine learning (ML), and the growth of 5G wireless communications all mean that the existing networks will be unable to scale for future demand.

The Move to 400G

The current standard for Ethernet networks is 100 Gigabit Ethernet (referred to as 100G, 100GbE, or 100GbE), the latest in many protocols adopted as data speeds have increased. As the name suggests, it supports data transfer rates of 100 gigabits per second (Gbps) and is governed by the IEEE 802.3 standard. It is widely adopted in data centers, high-performance computing environments, and other applications that process large amounts of data.

The current 100G and next-generation 400 Gigabit Ethernet (400G) are both high-speed networking standards that are used to transfer data between devices. However, there are some key differences between them.

The most apparent difference is speed. As the name implies, 400G Ethernet is four times faster than the existing system. Not only does this result in higher communication speeds, but it also creates greater bandwidth. The bandwidth of a networking standard refers to the amount of data that can be transferred over a given period. With the demands being placed on our modern communication systems, greater bandwidth is vital to support the latest data-intensive applications and services.

400G Ethernet has been created with the data center in mind. It has been designed to handle more data-intensive workloads, such as big data analytics, AI, and high-definition video streaming, which are becoming increasingly common in data centers.

Achieving Higher Performance

The adoption of new signal modulation techniques is key to the improved performance of the 400G network. Traditional data communications have depended on binary communications. Digital signals are transmitted in binary states (zeroes and ones), often referred to as non-return to zero (NRZ). To expand the capacity, the latest systems use a technique known as four-level pulse amplitude modulation (PAM4). PAM4 is a signal modulation technique that uses four different signal levels to represent data instead of two. With this technique, the capacity or bandwidth can be doubled, but at the cost of requiring specialized hardware and cabling. The reason that the hardware needs to be upgraded is to preserve signal integrity.

Signal integrity (SI) is the name given to the techniques and technology applied to preserve the quality of digital signals sent across wired, optical, or wireless media. For a signal to be received accurately, the medium over which it is sent must not degrade it to the point where the difference between the different states cannot be determined.

For traditional NRZ signals that are transmitted in two states, the voltage difference between the states is easier to detect. Therefore, the system is more tolerant of electronic noise or interference. However, PAM4 uses four different states, and the difference in voltage between each state is smaller. Consequently, the integrity of the signal is more at risk of interference. Designers must turn to more advanced technology to protect the SI.

As the medium over which the signals are sent has a significant impact on the performance of the system, the design of the transceivers, connectors, and cabling plays an essential role in preserving SI. The connectors used for 400G Ethernet are evolutions of the types used on older systems, often with new features.

New Form Factors

One such evolution is Quad Small Form-factor Pluggable Double Density (QSFP-DD), a compact, high-density transceiver module form factor that supports data rates up to 400Gbps. Developed from the QSFP28 module, QSFP-DD features twice as many channels as the older design but without an increase in overall size. When combined with the doubling of capacity achieved through PAM4 signaling, QSFP-DD can support the 400G network transmission for the newest systems.

The quest for more incredible speed cannot only be achieved by incorporating more channels into existing connectors. To generate the higher rates needed for 400G Ethernet, the processors require greater power and, thus, more heat.

To cater to this increased performance, the new Octal Small Form-factor Pluggable (OSFP) is a pluggable form factor with eight high-speed electrical channels that support 400Gbps. It is slightly broader and deeper than the existing QSFP design. It has an integrated heat sink that significantly improves thermal performance and enables modules with up to 15W power in a switch chassis without additional thermal management.

These new form factors are enabling system architects to take advantage of higher port densities. The latest-generation transceivers using QSFP-DD and OSFP devices offer higher port densities than previous generations, allowing data centers to conserve space and reduce costs. In addition, the superior performance of these new form factors enables system architects to scale their networks more efficiently to meet the growing demands of applications and services. This helps ensure that data centers continue operating effectively and efficiently as their needs evolve.

Barriers to Entry

With so much additional performance available, the benefits of 400G Ethernet are clear. However, moving from 100G to 400G Ethernet is not straightforward. The principal barrier to the adoption of this new technology is cost. Implementing 400G Ethernet requires significant investment in equipment and infrastructure. The cost of new transceivers, switches, and other devices is relatively high compared to previous generations of Ethernet. In addition, as 400G Ethernet is still relatively new, not all vendors can produce the necessary equipment.

The need for additional training also causes a significant cost impact. Making the most of the greater performance on offer requires a new set of skills, and organizations will need to make considerable investments in the training of their staff to deploy and manage 400G Ethernet networks correctly.

Organizations must also consider the compatibility of their existing networks when deploying new technology. The transceivers and connectors required may not be compatible with existing equipment, making it difficult for organizations to upgrade their networks to support 400G Ethernet.

System architects must also consider the impact of 400G Ethernet on power and thermal management infrastructure. The equipment delivering greater performance requires more power and generates more heat. The cost of upgrading existing power networks and the effort needed to provide sufficient cooling will be high.

Finally, many companies will be wary of adopting new equipment in the early stages of its development, and 400G Ethernet standards are still evolving. Companies may delay purchasing decisions because they are unable to determine which equipment and technologies comply with the latest standards. As this technology is still in its early stages, few existing customers are employing it. The lack of real-world testing can be a concern for companies who feel unable to assess its performance and reliability.

Beyond 400G

As powerful as 400G Ethernet is, it is the latest development on the path to the faster systems of the future. The next step after 400G is already being considered, with 800G and 1.6 Terabit Ethernet. These faster systems will be able to support even more data-intensive applications, such as real-time video streaming, virtual reality, and other applications that require extremely low latency and high bandwidth.

It is also important to remember that this new technology will also play a key part in the roll-out of robust 5G networks, as the high speed and low latency required for 5G communications are similar to the demands of 400G Ethernet.

Conclusion

400 Gigabit Ethernet is a relatively new technology, and its adoption is still in the early stages. Although not yet widely adopted, it is expected to gain broader adoption in the coming years.

The key drivers behind the adoption of this new technology will be the demands created by data-intensive applications, such as AI, cloud computing, big data analytics, and high-definition video streaming. These applications are becoming increasingly popular, and as a result, the demand for high-bandwidth, low-latency connections will also increase.

Some early adopters, such as large internet and cloud service providers, already use this new technology in their data centers. For other organizations, the relatively high cost of new equipment and the skills required to implement them to their full potential are significant concerns.

About the Author

David Pike is well known across the interconnect industry for his passion and general geekiness. His online name is Connector Geek.

Profile Photo of David Pike