Skip to main content

Powering Medical Ultrasound Imaging

By Chris Griffith and Rich Nowakowski, Texas Instruments

 

Medical ultrasound imaging can be used to visualize internal organs without puncturing the skin or introducing radiation as some other imaging systems like endoscope, computed tomography (CT), or X-ray imaging. Additionally, ultrasound is less expensive and more portable than non-invasive magnetic resonance imaging (MRI). The growth of ultrasound usage appears to be a strong trend for years to come.

Ultrasound block diagram

An ultrasound system (see Fig. 1) typically comprises several key building blocks that add to the power requirements. The ultrasound probe contains up to several hundred piezo-electric transducers which can covert outbound electrical signals into acoustic waves or inbound acoustic waves into electrical signals.

To create the electrical signals that will be input to the transducer, a transmit beamformer unit is used. The transmit beamformer typically is implemented in a field programmable gate array (FPGA) or digital signal processor (DSP). The transmit beamformer generates electrical pulses that are timed and scaled to illuminate specific areas within the body.

Key components of an ultrasound system.
Fig. 1: Key components of an ultrasound system.

These electrical signals from the transmit beamformer pass through a high-voltage pulser or high-voltage D/A converter (DAC) to create energy that excites the transducer element. A transmit / receive switch is placed between the pulser or DAC. During the transmission, it ensures that the low-voltage receive circuitry is protected from high voltages, since the receive path also needs connection to the transducer.

A piezoelectric transducer element converts these electric signals into acoustic waves that penetrate the body. These acoustic waves are reflected off the boundaries of various internal organs and return to the transducer.

Once these returning acoustic waves pass through the transducer, they become electric signals. These lower voltage receive signals need to be amplified, filtered, and converted to a digital format so an image can be created. Thanks to advancements in semiconductors, this all can be done in one device: the analog front-end (AFE).

The digital output is loaded into a receive beamformer that reconstructs the data. After the image is reconstructed it may have some video post-processing performed and put into a format that can be outputted to a display so the technician can view the result.

Point-of-load power

Many voltage levels need to be considered for an ultrasound imaging system, and understanding the power requirements early in the design phase can save time constructing the power architecture. When determining the system bus voltage, it is best to know the highest voltage level needed. The ultrasound transmit pulser may require the highest voltage level in the system with a peak current of several amperes to drive the transducer.

The most popular choice for an intermediate bus voltage is 12 V. A separate power supply may need to be implemented to generate a higher positive and negative voltage to provide power to the pulser. If the ultrasound has a battery-backup feature that may require a higher voltage to charge lead acid or a series/parallel combination of lithium-ion (Li-ion) batteries, then a 28 to 30-V intermediate bus voltage is a good choice.

There are many easy-to-use dc/dc switching regulators on the market that can accept this voltage level to provide point-of-load (POL) power for the display, digital processors, and analog circuits. Additionally, ultrasound imaging systems can be very susceptible to noise due to sensitive precision analog circuitry and the need of a clear display image. Dc/dc switching regulators with a frequency synchronization feature can be driven from a master clock frequency to eliminate beat frequencies that disturb analog and video signals.

Processor power

An ultrasound imaging system employs a combination of FPGA, DSP, and a microcontroller to implement the beamforming transmit and receive function, Doppler processing, and image processing. Powering the processors is straightforward, and manufacturers such as TI have tools available to suggest suitable power devices, such as the power and analog for processors and FPGA’s tool located at www.ti.com/processorpower.

However, a few important factors must be considered when powering performance processors. Processor manufacturers may specify a minimum and maximum voltage ramp time, and many dc/dc regulators feature an adjustable soft-start pin to program the voltage ramp time. If a soft-start pin is unavailable, choose a dc/dc regulator with a suitable preset soft-start time.

Processor datasheets may also provide recommended timing guidelines for core, I/O, phased-lock loop (PLL), and auxiliary power-up sequencing in their datasheets. While several distinct methods to power up-and-down voltage rails are available, sequential sequencing is most popular. This can be easily implemented by connecting the voltage regulator’s POWERGOOD pin to the ENABLE pin of another.

Sequential sequencing also allows multiple voltage rails to be staggered during turn-on to minimize inrush current as opposed to turning on all rails simultaneously. Some low-dropout regulators (LDOs) and switching regulators have a special sequencing or tracking pin that can accommodate almost any sequencing scheme

Lower processor-core voltages are driving the need for higher-accuracy dc/dc converters. New voltage regulators claim ±1% or better reference accuracy over temperature. Lower-cost voltage regulators may specify ±2% or ±3% reference voltage accuracy. Check the manufacturer’s datasheet for guarantees to ensure regulation accuracy meets processor requirements. Older dc/dc converters that have been reused for many years may not meet the voltage-accuracy needs of today’s latest processors.

Analog circuitry power

The ultrasound system’s main analog components are the AFE, ultrasound transmit pulser, and the ultrasound transmit/receive switch. These analog circuits, such as DACs, analog-to-digital converters (ADCs), and operational amplifiers (op amps) in high-precision instrumentation applications are very sensitive to noise and ripple.

Noise is characterized by spectral noise density (nV/√Hz) and output noise voltage (µVRMS). Power supply ripple rejection (PSRR) refers to the amount of ripple on the output coming from ripple on the input. Most designers choose a linear regulator to provide a clean voltage rail to maximize system performance. Linear regulators that advertise the PSRR and noise performance specifications on the front page of the datasheet are optimized to power noise-sensitive analog-integrated circuits.

An AFE, such as the AFE5808A, consists of an eight-channel voltage controller amplifier with a low-noise amplifier, a programmable gain amplifier, a CW mixer, an ADC, and other analog circuitry. The device requires several voltages, such as 1.8, 3.3, and 5 V to power the various circuitry blocks.

LDO regulators are suitable to power these AFE voltage rails since the current levels are low. To further improve efficiency and save the board, a switching regulator and an LDO are combined in one package that can power sensitive analog circuitry. For example, the TPS54120, a low-noise, power supply with integrated dc/dc converter and LDO supports up to 1A and can provide the high efficiency of a switching regulator and the high PSRR of an LDO from a 5- or 12-V bus with a low-noise output of 17 µVrms.

The ultrasound transmit pulser, such as the LM96550, contains eight high-voltage pulsers with integrated diodes generating up to ±50-V bipolar pulses with peak currents of up to 2 A, and pulse rates of up to 15 MHz. Since the transmit pulser also implements digital-to-analog conversion, separate voltage rails are required to power a level-shifter and low-voltage logic supply.

A split-rail power supply is required, and a step-down converter like the TPS54060 in an inverting buck/boost configuration easily generates the plus and minus voltage rails from the intermediate bus voltage. It is a good design practice to employ a low-current LDO on each rail to help remove any switching noise from the inverting buck/boost converter.

The ultrasound transmit/receive switch protects the AFE inputs of the low-noise amplifier (LNA) from the transmit channel’s high-voltage pulses. The input voltage is delivered from the transmit pulser’s output, and the output voltage to the LNA is ±0.7 V with the current clamped to 1 mA. Similar to the transmit pulser, the switch requires a split-rail power supply for the analog supply as well as a negative high-voltage bias supply. The bias supply needs to be the most negative power supply connected to the switch.

Ultrasound imaging systems comprise analog and digital integrated circuits that have different power considerations. Linear regulators can provide the low-noise performance for analog circuits. Switching regulators deliver higher efficiency and generally are more suitable for powering higher current, high-performance DSPs. Power solutions from Texas Instruments are available to combine the benefits of both switching and linear regulation to design a complete ultrasound imaging system.

About the Author

Texas Instruments Incorporated designs and manufactures analog technologies, digital signal processing (DSP) and microcontroller (MCU) semiconductors. TI is a leader in semiconductor solutions for analog and digital embedded and applications processing. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries.