Skip to main content

Object Tracking with PIR Sensors

New Tech Tuesdays

Join Rudy Ramos for a weekly look at all things interesting, new, and noteworthy for design engineers.

Published February 7, 2023

Motion detection refers to the process of detecting a change in the position of an object over time. This can be done using various techniques, such as infrared sensing, acoustic sensing, or image processing.

Humans perceive motion through visual and vestibular cues, with the brain using information from the eyes and inner ear to detect changes in the visual field to sense movement. Similarly, passive infrared (PIR) motion sensors detect changes in the infrared radiation (IR) emitted by all objects above absolute zero.

How Do PIR Sensors Work?

A PIR motion sensor primarily consists of two parts: a pyroelectric sensor that detects infrared radiation and an optical lens that focuses the infrared radiation onto the sensor. PIR sensors detect changes in infrared radiation (radiant heat) by measuring the objects’ temperature and surface characteristics in their field of view. The term "passive" in PIR refers to the fact that these devices do not emit energy to detect motion. Instead, they detect changes in the infrared radiation emitted or reflected by objects in their field of view. When an object, like a person, moves in front of a background, like a wall, the temperature at that point in the sensor's field of view increases from room temperature to body temperature and then back again. The sensor converts this change in incoming infrared radiation into a change in output voltage, triggering a detection signal to an alarm system or other device to indicate motion. PIR motion sensors are commonly used in security systems, lighting controls, and other applications where motion detection is needed. Additionally, objects that have similar temperatures but different surface characteristics may emit different infrared patterns, causing a detection when moved in relation to the background.

Demand for PIR Sensors

The market for PIR motion sensors is strong, with a wide range of applications, including security systems, lighting control systems, HVAC systems, and smart home devices. The market is expected to continue growing in the future as the demand for smart home and building automation products increases.

In this week's New Tech Tuesday, we'll look at the P1616 IR Emitter from ams OSRAM and the STEVAL-BLUEPIRV1 motion detector from STMicroelectronics and the central role they play in motion detection solutions.

PIR Sensor Solutions

ams OSRAM SFH 4172 OSLON® P1616 is a high-power infrared emitter in a clear silicone package. It has an 850nm centroid wavelength, an operating temperature range of -40°C to 105°C, and a 2kV ESD rating. The P1616 sensor is ideal for access control & security, body tracking, home/building/factory automation, and building lighting applications.

The STEVAL-BLUEPIRV1 evaluation board from STMicroelectronics is a wireless motion detector based on a PIR sensor and features Bluetooth® Low Energy wireless connectivity. The design uses IRA-S210ST01 by Murata and has a detection range of up to 5m. The whole design has been built by focusing on low-power consumption with an expected lifetime of around a year while powered via a CR2032 coin-cell battery.

Tuesday’s Takeaway

Motion is perceived by humans through a complex process, while PIR sensors detect changes in infrared radiation emitted by all objects. Increased demand for smart homes, building automation, and security systems is driving the market for PIR motion sensors. To meet this demand, designers will need to continue innovating and developing more sensitive, low-power, and cost-effective motion sensing solutions like those offered by ams OSRAM and STMicroelectronics.

About the Author

Rudy brings 35+ years of expertise in advanced electromechanical systems, robotics, pneumatics, vacuum systems, high voltage, semiconductor manufacturing, military hardware, and project management. Rudy has authored technical articles appearing in engineering websites and holds a BS in Technical Management and an MBA with a concentration in Project Management. Prior to Mouser, Rudy worked for National Semiconductor and Texas Instruments.

Profile Photo of Rudy Ramos