Riding the Waves of Analog to Digital Audio
New Tech Tuesdays
Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.
Published February 11, 2025
In this week’s New Tech Tuesday, we dive into the fascinating journey of how analog signals are converted into the crisp, clear digital audio we enjoy today. By unpacking the high-level stages of signal processing and conversion, we can better appreciate the engineering marvels that transform raw sound into immersive listening experiences.
Mechanics from Analog Signals to Digital Sounds
Converting analog signals into digital audio involves a series of carefully engineered steps. Each phase plays a crucial role in ensuring that the original sound remains authentic while benefiting from the precision and durability of digital formats.
Origins of Analog Signals
Analog signals are continuous waveforms that capture sound in its rawest form, such as from a musician’s instrument or recording microphone. While analog signals are rich in detail, they are also prone to distortion, noise, and wear over time, making preservation and reproduction challenging.
These limitations led to the need for digital conversion. The transition from analog to digital safeguards the integrity of the audio and enables advanced processing techniques that enrich the listener’s experience.
Digital Conversion Process
Digital conversion transformation ensures that the audio can be manipulated, stored, and transmitted with unparalleled accuracy. Figure 1 represents the conventional behavior of an analog-to-digital converter (ADC).[1]

Figure 1: An ADC peripheral is used to convert an external analog signal (voltage) into digital values for further processing in the digital domain. (Source: STMicroelectronics)
Sampling and Quantization
The first step in the digital conversion process is sampling, where the analog waveform is measured at specific intervals. Higher sampling rates (e.g., 44.1kHz for compact discs or 96kHz for studio recordings)[2] capture more data, resulting in better audio fidelity.
Following sampling is quantization, where each sampled point is assigned a numerical value. These values form a digital representation of the analog signal, preserving its key characteristics while enabling compatibility with digital systems.
Signal Processing and Enhancement
Once in digital form, the audio undergoes digital signal processing (DSP) to optimize its quality. DSP techniques such as filtering, equalization, and noise reduction help remove unwanted artifacts and enhance the listening experience.
Role of DSPs in Modern Audio
DSPs are key to modern audio systems. These powerful processors enable real-time adjustments that tailor audio output to specific environments or preferences. For instance, headphones with active noise cancellation (ANC) rely on DSPs to neutralize ambient sounds, delivering a pristine auditory experience.
Moreover, DSPs empower producers and engineers to experiment with effects, spatial audio, and dynamic range compression.
Acoustic Output Brings Sound to Life
The final stage in the journey is converting digital signals back into analog form. Digital-to-analog converters (DACs) perform this task, transforming numerical data into sound waves that resonate with listeners. Innovations such as planar magnetic drivers and high-resolution DACs continue to push the boundaries of what’s possible in audio reproduction.[3]
The Newest Products for Your Newest Designs®
This week’s New Tech Tuesday features products from STMicroelectronics and Analog Devices, showcasing innovative solutions for high-fidelity audio amplification and system evaluation.
The STMicroelectronics HFA80A is a highly efficient Class-D audio amplifier designed for bridge-tied load (BTL) configurations, offering a balance between performance and energy efficiency. With low distortion and high output power, it is ideal for driving speakers in portable and automotive audio applications.
The MAX98380 from Analog Devices delivers high-quality audio amplification with a digital input that supports versatile audio sources in compact designs. This Class D amplifier integrates a PWM modulator, a power stage, and a low-pass filter into a single chip, reducing design complexity. Its efficient power conversion and small footprint make it perfect for consumer audio devices, wearables, and IoT applications. Additionally, the MAX98380EVSYS evaluation system enables engineers to assess the performance of the MAX98380 in real-world applications.
Tuesday’s Takeaway
The transformation of analog signals into digital audio is a testament to the ingenuity of modern engineering. From sampling and signal processing to DAC-driven playback, every step ensures a faithful representation of the original sound. Whether you’re an audiophile or a curious learner, this process showcases the perfect harmony of technology and artistry.
Sources
[1]https://www.st.com/resource/en/application_note/an5012-analogtodigital-audio-conversion-example-using-stm32l4-series-microcontroller-peripherals-stmicroelectronics.pdf
[2]https://www.cambridgeaudio.com/usa/en/blog/what-is-high-resolution-audio
[3]https://bloomaudio.com/blogs/articles/whats-the-difference-between-dynamic-and-planar-magnetic-drivers