Skip to main content

The Rise of DC Microgrids

Efficiency, Implementation, and Regulatory Evolution

Image Source: malp/stock.adobe.com

By Adam Kimmel for Mouser Electronics

Published November 15, 2024

Renewable energy and electrification aren’t just on the way—they’re here. With them comes an increased share of the power load to direct current (DC) over alternating current (AC) power. A growing fraction of the combined residential and commercial power load in the US—between 60 and 75 percent—uses DC, driven by the adoption of electric vehicles and HVAC equipment with DC motors. This ratio starkly contrasts historical levels dominated by AC, with native DC loads accounting for around 32 percent as of 2019.[1]

This article examines the advantages of DC microgrids, an emerging infrastructure that transmits DC among application areas. It also explores the challenges and solutions involved in implementing DC microgrids and analyzes the evolving regulatory framework surrounding their adoption.

Advantages of DC Microgrids As Renewable Energy Expands

Microgrids are an emerging technology that combines the power flow management advantages of smart grids with smaller, decentralized energy generation. This approach moves power generation closer to where it is consumed for a more resilient, localized option to promote energy independence, especially in remote communities.

Energy Efficiency and Power Quality

DC microgrids offer significant benefits over traditional AC power systems. One of the most helpful advantages is improved energy efficiency by eliminating AC-to-DC conversion losses. This benefit is particularly relevant for systems that rely heavily on renewable energy sources, such as photovoltaic (PV) cells, which generate DC power without converting to AC. By eliminating the need for multiple conversions between AC and full DC loads, systems lose less energy, leading to more efficient power distribution.

Furthermore, DC microgrids provide improved power quality. The DC distribution system regulates voltage levels and improves power quality. Unlike AC systems, where voltage and frequency stability fluctuate, DC systems aim to maintain a consistent voltage, leading to more stable power delivery. Higher power quality makes DC microgrids well-suited for applications with sensitive electronics and critical systems that require high reliability and predictable, high-quality power.

Integration with Renewable Energy

DC microgrids naturally pair with renewable DC energy sources like solar and battery storage as well as some smaller wind and hydroelectric power stations.[2],[3] Renewable energy generators play a vital role in integrating renewable energy into DC microgrids, enhancing reliability and sustainability. Most renewable energy sources are already DC, matching source power with demand power type. This power match and ease of integration make DC microgrids ideal for environments where renewable energy is a primary power source.

Commercial and Residential Applications

A higher fraction of DC power devices means higher user efficiency and sustainability. Through microgrids, DC-DC can help companies achieve sustainability goals like net zero carbon emissions and reduce costs for consumers and building owners.

Another advantage of delivering high-efficiency electric power is enhancing the benefits of electrically driven technologies like heat pumps. Generally, heat pumps deliver two to four units of output power for one unit consumed;[4] however, the sustainability of this technology is tied to the source power. So, using high-efficiency electricity to drive a heat pump compounds the sustainability gain.

Challenges and Solutions in DC Distribution Systems

Implementing a reliable DC microgrid presents several challenges, particularly regarding voltage management and load balancing. In AC systems, transformers manage voltage changes. However, DC system engineers must rely on DC-DC converters to regulate voltage levels and ensure the system operates efficiently. Additionally, load balancing in these DC distribution systems can be complex, as these systems often operate in distributed networks with multiple energy generation and consumption points.

Key Technologies for Stability

Power flow management is essential for maintaining stability and efficiency in DC microgrids. Appropriately managing the electricity flow ensures a stable balance between power generation and consumption.

  • DC-DC converters: These converters help regulate the voltage across different parts of the microgrid. Stepping voltage levels up or down to meet demand ensures efficient energy delivery to the various loads within the microgrid.
  • Energy storage systems: Battery-powered energy storage systems allow excess renewable energy to be stored for use during periods of low source energy availability. This approach stabilizes the microgrid and enhances its reliability by ensuring continuous power availability despite the variability of renewable source energy.
  • Power management ICs: Smart power management integrated circuits (PMICs) and sensors monitor and control energy flow within the microgrid. These systems optimize load distribution, guard against overloads, and enable real-time adjustments based on consumption patterns.

Best Practices for Microgrid Design

Designing a DC microgrid involves several best practices that ensure efficiency and scalability:

  • Load profiling: It is critical to understand the specific power consumption patterns of the devices and systems connected to the microgrid. Accurate load profiling helps engineers design the microgrid to handle peak loads and ensure stable operation.
  • Hybrid systems: In some cases, microgrids that integrate AC and DC infrastructure (i.e., hybrid microgrids) may be necessary. These systems accommodate both legacy AC equipment and newer DC technologies.
  • Modularity and scalability: Designing microgrids that consider modularity ensures they can scale as energy needs evolve. This feature is especially important in commercial and industrial settings, where power demand can fluctuate over time at high load levels.

Regulatory and Standardization Needs for DC Microgrids

Like many new technologies, regulations can both enable and hinder adoption, depending on location. Understanding today’s regulatory landscape—and its likely future—is essential when considering microgrid adoption.

Current Regulatory Landscape

One of the main challenges facing commercial adoption of DC microgrids is the relative lack of federal regulations, codes, and standards. The US Federal Energy Regulation Commission (FERC) regulates interstate sales and rates (among other factors) and in 2020 issued Order No. 2222, designed to facilitate distributed energy resources (DERs)—including microgrid operators—introduction into electricity markets.[5] Unlike AC distribution systems, which have well-established metering and power quality standards, DC microgrids currently lack uniform regulations for metering consumption and ensuring power quality. This gap has created uncertainty for organizations looking to implement DC systems, as compliance requirements may vary depending on the region.

International Standards and Regional Variations

Several regions are beginning to develop standards for DC microgrids, but progress is uneven. In Europe, regulators have started defining standards for DC systems, mainly for commercial and industrial applications.[6] In contrast, the United States is still in the early stages of developing DC-specific regulations. Many of these are state-driven, potentially due to the local nature of the power solutions.

The National Association of State Energy Officials (NASEO) and the National Association of Regulatory Utility Commissioners (NARUC) created a repository for resources and guidance for developing state microgrid policies, programs, or regulations.[7]

International organizations like the International Electrotechnical Commission (IEC) and the Institute of Electrical and Electronics Engineers (IEEE) are actively working on creating standards for DC microgrids, which will help streamline their implementation and reduce regulatory barriers.[8],[9]

Future Regulatory Requirements

As DC microgrids continue to gain traction, regulatory bodies need to address additional parameters around microgrids:

  • Metering accuracy: Developing clear standards for metering DC power consumption would ensure accurate billing and monitoring of energy use.
  • Voltage and power quality: Regulators must define acceptable voltage ranges and power quality standards for DC systems to ensure their safety and reliability.
  • Integration with existing infrastructure: Regulatory frameworks must facilitate the integration of DC microgrids with existing AC infrastructure to enable hybrid systems and ensure smooth transitions.

Future targets of regulatory action could include interconnection and licensing, tariffs that drive proper behaviors in support of sustainability, ownership guidelines, and compliance reporting structure.

DC Microgrid Application Spotlight: Energy Harvesting

DC microgrids operating with renewable energy sources can benefit from energy harvesting. Perhaps the main challenge with renewable energy systems is the variability in energy generation, such as the fluctuation of sunlight or ideal wind conditions. While energy storage systems (like batteries or thermal bricks) can mitigate some of these issues by storing excess energy for later use, integrating energy-harvesting technology into the microgrid can provide incremental stability and efficiency.

For example, small-scale energy harvesters can capture energy from the environment when solar or wind energy generation is low. This captured energy can power the microgrid’s sensors, Internet of Things (IoT) devices, or low-power communications systems. Adding supplemental power recovery reduces the reliance on stored battery power and maximizes the use of available energy in the system. The decentralized nature of DC microgrids also means that this harvested energy can be distributed directly where needed without requiring the inefficiencies of AC-to-DC power conversion alone.

While energy harvesting shows clear potential, engineers must address outstanding technological challenges to integrate it fully into DC microgrids. The primary challenge lies in these systems’ relatively low power output, often measured in milliwatts. While such levels are sufficient for low-power applications like sensors and communication systems, they are not enough to handle larger loads. As a result, energy harvesting must be viewed as a complementary technology that augments DC microgrids rather than as a primary energy source.

DC microgrids will require sophisticated power-management systems capable of efficiently capturing and distributing the harvested energy to support the integration of energy harvesting. These systems must also ensure seamless transitions between harvested, stored, and grid power so that devices and systems remain operational without interruption.

The Path Forward for DC Microgrids and Renewable Energy Integration

DC microgrids can transform power distribution, much like how edge computing has improved data transmission. Microgrids deliver significant efficiency and quality enhancements, adding a substantial renewable energy application to respond to the growing demand for DC-powered devices. These systems offer measurable benefits in energy efficiency, lower cost, power quality, and integration with renewable energy sources. However, their widespread adoption depends on overcoming technical challenges and establishing clear regulatory frameworks.

As countries and states develop ways to regulate and integrate DC microgrids into the power system, the technologies and renewable energy that use them are well suited for massive growth in the coming years.

 

Sources

[1]https://www.usgbc.org/articles/new-leed-pilot-credit-encourages-energy-savings-dc-power-systems
[2]https://www.energy.gov/energysaver/microhydropower-systems
[3]https://windexchange.energy.gov/small-wind-guidebook
[4]https://www.energy.gov/energysaver/air-source-heat-pumps
[5]https://www.naruc.org/core-sectors/energy-resources-and-the-environment/der-integration-compensation/
[6]https://setis.ec.europa.eu/document/download/d312944b-df45-4ebb-b2bd-d8616d13bbf4_en?filename=SET-Plan-LVDC-Implementation-Plan-12sep2024-endorsed.pdf
[7]https://www.naruc.org/core-sectors/energy-resources-and-the-environment/microgrids/
[8]https://www.iec.ch/energies/minigrids-microgrids
[9]https://ieeexplore.ieee.org/document/9646866

About the Author

Adam Kimmel has nearly 20 years as a practicing engineer, R&D manager, and engineering content writer. He creates white papers, website copy, case studies, and blog posts in vertical markets including automotive, industrial/manufacturing, technology, and electronics. Adam has degrees in Chemical and Mechanical Engineering and is the founder and Principal at ASK Consulting Solutions, LLC, an engineering and technology content writing firm.

Profile Photo of Adam Kimmel