Skip to main content

From Concept to Gadget: Building Embedded Systems That Ship

(Source: ROMBIX STUDIO/stock.adobe.com)

Published April 24, 2026

Starting a new embedded electronics project can be both exhilarating and overwhelming. It’s an opportunity to learn new techniques, explore new components, and build something tangible. But before the first line of code is written or the first printed circuit board (PCB) trace is routed, a significant amount of groundwork must be done. Requirements need to be defined, architectures planned, budgets and schedules agreed upon.

There are entire textbooks on product development, so the goal of this blog is not to be exhaustive. Instead, it provides a practical framework for low-volume embedded devices, such as a gadget retailing for around $100USD. By keeping scope and complexity constrained, we can focus on the essential steps required to move from concept to prototype to small-batch production.

Step 1: Requirements define the "what" and "why"

Though it is tempting to jump straight into wiring sensors to a development board, successful projects begin with clear requirements. These requirements become the foundation for every decision that follows.

Identify the problem and use case

Start by identifying the problem and use case. Ask, “What is the device meant to do, and who will use it? A consumer device demands simplicity, safety, and polish. A tool for trained technicians can assume more technical knowledge and tolerate complexity. The intended user strongly influences interface design, durability, documentation, and support expectations.

Define functional requirements

Once the problem and use case are clearly understood, the next step is to translate that understanding into concrete capabilities the device must deliver. List the core capabilities the device must provide, such as sensor ranges and accuracy, update rates, battery life, physical size, operating environment, cost targets, and any communications needs. Environmental factors matter—outdoor use implies temperature and moisture concerns, while industrial settings may require electrical noise tolerance.

Consider non-functional requirements

Beyond what the device does, it’s equally important to define how well it must do it. This is where non-functional requirements come into play. These include safety expectations, reliability goals, aesthetics, regulatory constraints, maintainability, and upgrade paths. Examples include “operate continuously for one year without reboot” or “support field firmware updates.”

Plan for verification early

Because each requirement should be testable, verification planning should happen in parallel with requirements development. If you specify eight hours of battery life, plan a discharge test. If operating down to 0 °C is required, plan a cold test. Thinking about validation early often reveals hidden needs, such as calibration procedures or diagnostic indicators.

For critical projects, a lightweight failure mode analysis can be invaluable. Asking “what happens if this fails?” often leads to additional requirements such as fail-safe behavior or user alerts.

Document your requirements—whether in a formal document or a notebook—and ensure each one ties back to a purpose and a verification method. Clear requirements prevent scope creep and keep development focused.

Step 2: Architecture and design (plan the "how")

With requirements clearly defined and tied to verification, attention can shift from what the device must do to how it will do it. This is the role of system architecture and design.

System architecture

Divide the system into functional blocks: sensing, processing, power, user interface, and communications. A simple block diagram helps visualize data and power flow and highlights integration challenges early.

Decide on core components. A microcontroller offers efficiency and low power consumption, while a Linux-based single-board computer may accelerate development but increase cost and power draw. Wireless modules can simplify certification and reduce development time. Every choice involves tradeoffs.

Hardware design considerations

Select hardware components carefully, verifying voltage compatibility, interfaces, addresses, packages, and availability. Read datasheets thoroughly and collect application notes and reference designs—they save time later. Some key Design for Excellence/X (DfX) principles to keep in mind:

  • Design for Manufacturability (DFM): Avoid exotic parts and follow good PCB practices.
  • Design for Assembly (DFA): Minimize part variety and assembly complexity.
  • Design for Test (DFT): Include test points and accessible programming interfaces.

Mechanical integration matters even at this stage. Ensure the PCB fits the enclosure, the mounting holes align, the connectors are accessible, and the cables are strain-relieved. Simple 3D models or even printed templates can prevent costly surprises.

Power design deserves special attention. Calculate power budgets, especially for battery-powered devices, and decide early on charging, regulation, and power-management features.

Software architecture

When planning the software architecture, choose a platform you can deliver with. C/C++ offers efficiency and control. CircuitPython or MicroPython accelerates iteration but requires more resources. Rust offers memory safety at the cost of a steeper learning curve. The “best” option is the one that fits the project and team.

Determine whether a real-time operating system (RTOS) is needed. Simple devices may run happily on bare metal, while systems with multiple time-critical tasks may benefit from FreeRTOS or Zephyr.

Though Internet of Things (IoT) devices are all the rage, think about if a connection to the internet is really needed. Connectivity adds value but significantly increases complexity. If the device doesn’t truly need internet access, leaving it offline avoids security, privacy, and maintenance challenges. If IoT is justified, plan for encryption, authentication, and long-term update strategies from day one.

(Remember,) Project organization is crucial. Use version control for firmware, schematics, PCB files, and documentation. Decide early whether the project will be open source or proprietary and ensure licenses align with that choice.

By the end of this step, you should have a clear technical roadmap, component selections, and a coherent plan for hardware and software integration.

Step 3: Prototyping and development (build, break, improve)

Prototyping turns plans into reality and exposes assumptions. During the prototyping and development stage(s), follow the principles outlined below.

Start simple

Start simple when prototyping. Use development boards and breadboards to validate sensors, displays, communications, and power consumption before committing to custom hardware. Early integration testing often reveals issues such as resource conflicts or library limitations.

Develop incrementally

Bring up the system in stages: verify the toolchain, test individual peripherals, then integrate subsystems. Small, testable milestones make debugging manageable.

Prototype PCB design

Once subsystems work, design a prototype PCB. Be sure to double-check pinouts, footprints, and power routing. Run design rule checks and review the layout carefully. Printing the board at 1:1 scale can catch mechanical issues. For low-volume boards, services like OSH Park, PCBWay, JLCPCB, and Seeed Studio offer affordable, high-quality fabrication. Choose based on board size, quantity, and turnaround time. Consider the assembly strategy. Through-hole parts are forgiving, while surface-mount parts save space. Use package sizes you can reliably assemble or leverage low-cost assembly services if needed.

Bring up methodically

Test the power supply first, then program the microcontroller. Add peripherals one at a time, verifying functionality at each stage. Expect bridge wires and fixes on early revisions. Be sure to document them for the next spin. Firmware development proceeds alongside hardware testing. Early code may be diagnostic-heavy, evolving toward production behavior over time. Source control is invaluable during this phase. Iteration is normal. Each prototype teaches you something and reduces risk.

Step 4: Testing and validation (prove it works)

Testing confirms that the design meets requirements and behaves reliably under real-world conditions.

Verify against requirements

Test each requirement explicitly: accuracy, battery life, environmental limits, durability, and performance. Document results, even for small projects.

Test edge cases and failures

Power cycling, brown-outs, sensor disconnections, communication dropouts, and environmental stress can reveal weaknesses. It’s better to discover them in the lab than in the field. Adopt a failure mode and effects analysis (FMEA) mindset during testing. Ask what happens when components fail or users make mistakes. Ensure failures are safe and detectable.

User feedback

Let representative users try the device. Observing real interactions often uncovers usability improvements that engineers overlook. Refine the design based on findings. Some fixes may require another prototype iteration; others can be addressed in firmware or documentation.

Step 5: Production, launch, and support

With a validated design, focus shifts to delivering a real product.

Finalize the design

Incorporate fixes, clean up firmware, and freeze files for production.

Plan low-volume manufacturing

For very small runs, in-house assembly may be practical. For larger quantities, turnkey assembly services can save time and improve consistency. Order extra components to account for losses.

Manage the supply chain

Check component availability and life cycles early. A single unavailable part can stall production.

Enclosures and labeling

Finalize mechanical designs, ensuring proper fit and alignment. Plan labeling, serial numbers, and branding.

Regulatory considerations

In the U.S., most electronic products require FCC compliance; devices with radios face stricter requirements. In the EU, CE marking is mandatory for most electronics. Using pre-certified wireless modules can significantly reduce cost and complexity. Even for low volumes, understand the legal implications of skipping certification.

Documentation and logistics

Prepare user guides, assembly instructions, and test procedures. Plan packaging and shipping to protect the product and satisfy customs requirements if shipping internationally.

Support and lifecycle

Expect post-launch support. Plan for firmware updates, repairs, and long-term component availability. Responsible design also considers end-of-life and recycling.

Conclusion

Embedded product development is inherently iterative. Requirements, design, prototyping, testing, and production often overlap and inform one another. A structured approach doesn’t limit creativity. Rather, it channels it into steady progress, reducing costly surprises.

Whether you’re building a commercial IoT device or a personal project, taking time to define requirements, design thoughtfully, prototype intelligently, test thoroughly, and plan for real-world deployment dramatically increases your chances of success. Few experiences match the satisfaction of turning an idea into a tangible, working product. With a solid roadmap, that journey becomes both manageable and rewarding.

About the Author

Michael Parks, P.E. is the owner of Green Shoe Garage, a custom electronics design studio and technology consultancy located in Southern Maryland. He produces the S.T.E.A.M. Power podcast to help raise public awareness of technical and scientific matters. Michael is also a licensed Professional Engineer in the state of Maryland and holds a Master’s degree in systems engineering from Johns Hopkins University.

Profile Photo of Mike Parks