Skip to main content

Raspberry Pi 5 Unveiled with Pre-Orders Available at Mouser.com

Image Source: Mouser Electronics

By Mouser Technical Content Staff with OpenAI ChatGPT v4

Published September 29, 2023

The Raspberry Pi Foundation has taken the tech industry by storm with the surprise release of their latest innovation, the Raspberry Pi 5. Destined to be a hot-ticket item from the start, the new iteration features groundbreaking silicon at its heart. Now available to order from Mouser Electronics, the Raspberry Pi 5 is a game-changer with a few new tricks up its sleeve.

The Raspberry Pi Foundation has navigated countless challenges over the years, from production woes to supply chain disruptions. But their unwavering commitment to delivering computing innovation to all has brought us to this pivotal moment.

Introducing the Raspberry Pi 5: A Marvel of Custom Silicon

The Raspberry Pi 5 is based on the Broadcom BCM2712, which houses a quad-core 2.4GHz 64-bit Arm® Cortex®-A76 processor. However, the standout component here is the RP1, a proprietary I/O controller crafted entirely in-house by the Raspberry Pi team. This custom chip assumes a pivotal role in furnishing USB 3.0, Ethernet, GPIO, MIPI display, and MIPI camera ports. The inclusion of the RP1 custom I/O chip not only adds stability to the Pi 5's manufacturing process but also optimizes power consumption by integrating only the most critical circuits into the chip. 

But the excitement doesn't stop there. Beyond custom silicon, the Raspberry Pi 5 introduces a four-lane PCIe 2.0 interface, streamlining high-speed peripheral connections. It also boasts Bluetooth® 5.0 with Bluetooth Low Energy, dual-band Wi-Fi®, and Gigabit Ethernet, granting users the flexibility to choose between wired and wireless connectivity. Moreover, the Pi 5 extends support for Power over Ethernet (PoE), enabling users to power the board via Ethernet, alongside a USB Type-C port for alternative power sources. 

While the board seamlessly integrates a real-time clock (RTC), the absence of an onboard battery necessitates using a networked time server to maintain time accuracy during power disruptions. Fortunately, users can power the RTC externally through a supercapacitor or small battery, ensuring precise timekeeping even in power outage scenarios. 

Power management receives an upgrade with the Renesas DA9091 power management IC, capable of supplying up to 20A to the BCM2712 for high-performance processing. The PMIC and Raspberry Pi 27W power supply should reduce or eliminate power warnings in most scenarios.

Raspberry Pi 5 Specifications

  • Broadcom BCM2712 2.4GHz quad-core 64-bit Arm Cortex-A76 CPU featuring cryptography extensions, 512KB per-core L2 caches, and a 2MB shared L3 cache.
  • VideoCore VII GPU, supporting OpenGL ES 3.1, Vulkan 1.2
  • Dual 4Kp60 HDMI display output with HDR support
  • 4Kp60 HEVC decoder
  • LPDDR4X-4267 SDRAM (4GB and 8GB available at launch)
  • Dual-band 802.11ac Wi-Fi
  • Bluetooth 5.0/Bluetooth Low Energy
  • microSD card slot, with support for high-speed SDR104 mode
  • 2 × USB 3.0 ports, supporting simultaneous 5Gbps operation
  • 2 × USB 2.0 ports
  • Gigabit Ethernet, with PoE+ support (requires separate PoE+ HAT)
  • 2 × 4-lane MIPI camera/display transceivers
  • PCIe 2.0 x1 interface for fast peripherals (requires separate M.2 HAT or other adapter)
  • 5V/5A DC power via USB Type-C, with Power Delivery support
  • Raspberry Pi standard 40-pin header
  • Real-time clock, powered from external battery
  • Power button

To see how these specs stack up against the Raspberry Pi 4, check out this infographic.

Conclusion

The introduction of the Raspberry Pi 5 heralds yet another innovation from the Raspberry Pi Foundation. The inclusion of the RP1 custom I/O chip not only adds stability to the Pi 5's manufacturing process but also optimizes power consumption by integrating only the most critical circuits into the chip. 

The possibilities are boundless with the Raspberry Pi 5. Be a part of this journey by taking advantage of Mouser’s pre-orders for the Raspberry Pi 5, available now!

About the Author

Mouser, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.

Profile Photo of Mouser Technical Content Staff