Skip to main content

CoAP Boosts Power and Resource Efficiency for the IoT

(Source: Truprint/stock.adobe.com; generated with AI)

Internet of Things (IoT) systems consist of many components and layers. Sensors detect data, which are then transferred through nodes that act as gateways to establish internet connectivity for the sensors. The nodes connect to various servers and edge computing systems to transmit the data to cloud servers, where it can be stored and analyzed.

However, many of the devices within IoT systems need to have limited footprint, central processing unit (CPU), memory, or power resources. These devices' limited functionalities mean they can become constrained, which is particularly true for IoT nodes. Multiple constraints within the nodes can exacerbate each other. Further, constrained nodes in IoT systems can cause the overall network to become constrained, leading to unreliable channels and a limited and unpredictable bandwidth.

The tight limits on different functional factors of IoT nodes create hard upper bounds on state, code space, and processing cycles. When constrained nodes exist in IoT systems, developers use several different protocols to improve the nodes' connectivity with each other and the wider network.

One example is the Constrained Application Protocol (CoAP), a client-server protocol modeled on Uniform Resource Identifiers (URIs) and Hypertext Transfer Protocol (HTTP) that ensures seamless communication in a constrained network or device. CoAP uses network resources efficiently to accommodate low-power devices and devices with limited computational capacity or intermittent connectivity. It can support multicast communication and has become an essential protocol for IoT systems.

This blog explores how CoAP aligns with the low-power and low-resource requirements of IoT networks by saving power and optimizing communication processes.

What Is CoAP?

CoAP is a web transfer protocol specifically designed for use with IoT systems, addressing the resource constraints in bandwidth, memory, and processing power. Unlike other protocols, CoAP has been designed with a minimalist approach that balances both functionality and resource conservation.

CoAP is based on a Representational State Transfer (RESTful) architecture and adheres to specific constraints that allow it to function effectively across large, distributed networks. By leveraging RESTful principles, CoAP treats data and operations as resources accessible through a uniform interface. This design promotes strong interoperability among devices and enables developers to create applications using familiar HTTP methods to interact with CoAP resources.

CoAP has a small base specification, but additional functionalities can be added when required. It operates using a User Datagram Protocol (UDP) as the underlying transport mechanism. UDP is a simple and connectionless transmission protocol, meaning it does not require an internet connection to be established before the data are sent. This feature makes it ideal for IoT systems that send small amounts of data quickly. Overall, the use of UDPs provides a request-response interaction model between endpoints that enables a high degree of interoperability and fast communication between devices in an IoT network.

CoAP has primarily been designed for machine-to-machine (M2M) applications, including smart energy, smart home automation, healthcare, wearables, and industrial IoT (IIoT) applications. In all these areas, it supports constrained nodes and networks while cooperating with HTTP through proxies. Mechanisms are in place to ensure that messages are delivered under limited network connectivity or low device power. This is why CoAP is a key protocol for IoT networks, as it can offer a high degree of assistance in challenging network environments, which is common for most IoT systems.

How CoAP Addresses Constrained Node Limitations in IoT

CoAP emerged as a protocol in the IoT space as a direct response to the limitations of traditional protocols in constrained devices and networks. Traditional networks like HTTP are resource-intensive, so they require more memory consumption, processing power, and bandwidth. For constrained devices that have tight resource limitations, traditional protocols can become burdensome and limit the operational efficiency of the IoT network. The reduced overheads from using UDP mean that communication and responsiveness can be improved in constrained networks, unlike traditional protocols that are based on Transmission Control Protocol/Internet Protocol (TCP/IP).

Like HTTP, CoAP uses a request-response model, but the modifications within the CoAP protocol make it more suitable and tailored for use with constrained networks compared to HTTP. The lightweight nature of the communication framework within CoAP protocols enables different IoT devices to seamlessly interact with each other while conserving energy and resources. CoAP achieves this partially through the observation of resource changes in the network. This approach prevents the need to continuously poll for updates, which in turn significantly reduces the level of unnecessary data exchange, saving power in the process.

CoAP also uses a more flexible messaging distribution approach that supports both unicast and multicast communication. Unicast communication is a direct, one-to-one communication between a client and a server for directing specific queries or commands to and from a single device. CoAP's multicast nature enables messages to be sent to multiple devices simultaneously, which reduces the need for many separate individual communications. This multicast transmission optimizes network usage and reduces overall communication overhead, conserving energy and resources, which enables the system to run more efficiently.

Pros and Cons of Using CoAP over Other Protocols

Other protocols, including Message Queuing Telemetry Transport (MQTT) and HTTP, are used alongside COAP in IoT systems. Compared to other, more established protocols, CoAP offers several advantages, while also coming with some disadvantages.

Some of the key advantages of CoAP include:

  • Minimalist design intended for IoT that conserves resources for lower power devices and networks
  • Lower communication overheads than HTTP
  • Lightweight architecture that allows the protocol to be scaled and used across many IoT devices and applications
  • Similar behavior to HTTP, offering familiarity for many developers and users
  • Flexible and dynamic
  • UDP operation that does not require an established connection before sending data
  • A binary encoding scheme that is more efficient than HTTP text-based encoding, saving bandwidth and increasing communication speed
  • Stateless communication, where each request from client to server is processed independently without any knowledge of previous requests, making it more robust and resilient to failures that arise from individual requests
  • Multicast communication that can send information to multiple devices simultaneously

Despite its specific advantages for IoT applications, CoAP does have disadvantages when compared to more established techniques, including:

  • Possible difficulty traversing firewalls (as compared to MQTT)
  • Can be used to amplify distributed denial of service (DDoS) attacks.
  • Less mature than other protocols, with fewer tools and libraries available for developers
  • Problems with Network Address Translation (NAT) due to the UDP not establishing a connection before sending data
  • Susceptibility to fragmentation when the message is too large to fit into a single packet and must be divided up, leading to decreased efficiency

Conclusion

The IoT landscape continues to expand and now encompasses many areas and industries, from automated manufacturing to smart homes. The small nature of IoT devices means that many of them have low power and low resource requirements, which can be a challenge for many traditional protocols like HTTP. As a result, CoAP has become an essential protocol for realizing more efficient communication and data transfer, filling the gap to solve some of the network limitations within IoT where more traditional protocols have struggled.

In IoT, CoAP’s primary role is to facilitate efficient and adaptable communications across constrained devices and, in turn, constrained networks through a lightweight communication framework. Many different aspects of the protocol save energy and resources, making it an optimal choice for IoT—for the most part. While CoAP has some disadvantages compared to established protocols, it has been specifically designed for IoT systems and has many considerable benefits that align with the unique low-power and low-resource requirements of IoT networks.

About the Author

Liam Critchley is a writer, journalist and communicator who specializes in chemistry and nanotechnology and how fundamental principles at the molecular level can be applied to many different application areas. Liam is perhaps best known for his informative approach and explaining complex scientific topics to both scientists and non-scientists. Liam has over 350 articles published across various scientific areas and industries that crossover with both chemistry and nanotechnology. Liam is Senior Science Communications Officer at the Nanotechnology Industries Association (NIA) in Europe and has spent the past few years writing for companies, associations and media websites around the globe. Before becoming a writer, Liam completed master’s degrees in chemistry with nanotechnology and chemical engineering. Aside from writing, Liam is also an advisory board member for the National Graphene Association (NGA) in the U.S., the global organization Nanotechnology World Network (NWN), and a Board of Trustees member for GlamSci–A UK-based science Charity. Liam is also a member of the British Society for Nanomedicine (BSNM) and the International Association of Advanced Materials (IAAM), as well as a peer-reviewer for multiple academic journals.

Profile Photo of Liam Critchley