Power Density vs. Power Efficiency

By Robert Huntley, for Mouser Electronics.
Updated on April 6, 2020 (Originally Published September 4, 2019)
Power-conversion efficiency is a headline metric, with module manufacturers vying with each other to show decimal-point improvements in the plus-95-percent figures under carefully selected conditions. Evermore complex conversion topologies are used to achieve these figures, such as phase-shifted full bridges (PSFBs) and LLC converters. Diodes are being replaced by metal-oxide-semiconductor field-effect transistors (MOSFETs) for lower losses wherever possible, and wide band-gap (WBG) devices are being hailed as the semiconductor of choice for the future with their spectacular switching speeds.
End users, however, look at the bigger picture and care more about the efficiency of their whole system or process in its ability to maximize profits while complying with environmental obligations. They understand that concentrating on incrementally reducing losses in one small element of the power-conversion process does not necessarily lead to significant overall cost savings or environmental benefit when all lifetime costs are factored in. On the other hand, packing more power-conversion equipment into a smaller volume — increasing its “power density”— can use factory or data center floor space more efficiently and produce more output with existing overhead costs.
Here, we examine the real costs of chasing percentage points of power conversion efficiency in energy saved, acquisition/disposal costs, and cabinet/floor space utilization compared with increasing power density and the system-efficiency improvements that can follow.
Maximizing Efficiency While Minimizing Costs
In the power electronics world, efficiency is a term that is easy to conceptualize — 100 percent equals good, zero percent equals bad, right? But you have to carefully set your reference point: A data center is close to zero percent electrically efficient overall — just about all power it draws from the grid is converted into heat in server blades, their power supplies, and the electronics in cooling systems. It might then be more efficient to convert the dollar value of electricity into dollar revenues, and the same is true of most industries. You wouldn't expect otherwise, so if you want to save costs and the planet while making money, the real issue is how you minimize the total power draw while maximizing productivity.
Data center managers know this and face daily pressure to increase data-processing capacity and speed while keeping the electricity bill as low as possible and getting payback from capital investment. They have little choice but to add servers in increments of many kilowatts of dissipation, but can calculate the monetary value added to capacity and offset that against the extra energy and capital costs. In industry, if another 100kW motor is needed, it is to produce more saleable output and the motor drive and its power supply is the unavoidable overhead. In all industries, power supplies are a necessary evil that add no commercial value in themselves, so every operating expense and watt dissipated in them is seen as reducing the bottom line. The spotlight, therefore, naturally turns on the power electronics manufacturers, with pressure to reduce losses by increasing electrical efficiency.
Efficiency is Relative
Power conversion efficiency seems easy to define — we can all quote the formula “power out divided by power in, as a percentage,” with the difference between the two dissipated as heat in the power converter. The problem is that efficiency is meaningless without quoting power levels and how they vary with operating and environmental conditions, leaving “efficiency” as only a comparative measure between converters. It is then open to “creative” specifications, picking out the sweet spots that show the equipment in the best light. Few converters are operated near their maximum power ratings, so efficiency is normally designed to peak at around 50 percent to 75 percent of maximum-rated load with some curve, which must fall off to zero efficiency at zero load. At light load, there can be huge variability between converter designs, so under idling conditions, one power supply might dissipate several times that of another (Figure 1). At 5 percent load, the converter represented by the orange line is dissipating more than three times the one for the blue line. Light load losses, therefore, make a significant difference to total energy draw.

Figure 1: Efficiency at light load can vary widely between otherwise similar power converters. (Source: Mouser)
Fortunately, standards set the shape of the efficiency curve, such as the “80-PLUS initiative” with its various levels. “Titanium” is the highest, demanding minimum 94 percent efficiency at 50 percent load and 90 percent at 10 percent load. These are for 115V systems; the figures for 230V are 96 percent and 90 percent, respectively (Table 1).

Table 1: The table shows the 80-PLUS initiative targets for 115V systems. (Source: Wikipedia)
These limits are quite tough to achieve. Achieving the Titanium level at 94 percent means reducing losses in the power supply by three-quarters. At a mere 14 percent increase in efficiency, a kilowatt-rated supply has to reduce losses from 250W to 64W. This is not achieved by fine-tuning existing designs and has necessitated a radical rethink of converter topologies. Diodes are dropped in favor of synchronously driven MOSFETs, PSFB, and LLC resonant topologies are used to limit dissipation during switching transitions, and new semiconductor technologies have arrived, such as silicon carbide (SiC) and gallium nitride (GaN) for faster switching without a dissipation penalty. Even the humble bridge rectifier of the mains has morphed into a hybrid arrangement of MOSFETs that also form part of the necessary power-factor correction circuitry. All of this does not come cheap and without the "risk of the new." Still, customers and power supply manufacturers are in a spiral of supply and demand for higher efficiency figures, pushing toward 99 percent and beyond.
The Cost of a Small Improvement
As power conversion efficiencies approach 100 percent, difficulty increases exponentially (Figure 2). From 97 percent to 98 percent means decreasing losses by a third; 98 percent to 99 percent means decreasing losses by a further half. Cutting losses by 50 percent in any converter design might force a complete restart from scratch, with the only route to use more complex techniques and more expensive components, often at the expense of size. A 1kW supply is only dissipating 20.4W at 98 percent efficiency. How much is the huge effort worth to hit 99 percent and 10.1W loss? Think about the load taking 1kW — you would get a 10.1W saving by reducing it by 1 percent. How much design effort would that take?

Figure 2: Losses vs. efficiency in a 1kW power converter. (Source: Mouser)
Of course, all energy savings are worth having, but you need to look at the bigger picture. According to the Rocky Mountain Power company, the average price paid for industrial electricity in the US is about 7 cents per kilowatt-hour. If the 1kW power supply lifetime is, say, five years or about 44,000 hours at 100 percent uptime, a reduction of 10.1W saves about $31 (USD), while the load power is costing over $3,100 (USD). Changing out the power supply has an acquisition cost, purchasing and qualification overhead, installation cost, and a carbon footprint associated with typically hundreds of components, packaging, and transportation. Then there are disposal costs for the old equipment, and the functionality risks with new, cutting-edge products. It's difficult to see how this offsets the $31 (USD) in savings compared with keeping previous generations of power supplies in place, assuming reliability is still adequate. Pursuit of high efficiency for its own sake can be an expensive business.
Managing Temperature for Power Density
Perhaps it's worth improving power converter efficiency to reduce internal temperatures and improve calculated life/reliability, but this only works if the case and cooling remain the same. There is an old rule of thumb that the lifetime of electronics reduces by a factor of two for each 10°C rise, and according to reliability handbooks, semiconductor failure rate increases by about 25 percent and capacitors by about 50 percent for a 10°C rise. However, modern electronics are extremely reliable and durable, so these are percentage changes from a very long lifetime and high-reliability figures anyway. Power electronics cooling has historically been set to maintain an ideal inlet temperature of around 21°C in data centers, for example, but research by Intel® and others has shown that this can be increased without significant effects on system reliability. A report by American Power Conversion™ (APC) quoting the American Society of Heating and Air-Conditioning Engineers (ASHRAE) predicts just a 1.5 times increase in overall equipment failure rate for an inlet air temperature rise of 20°C to 32°C (68 to 90°F) (Figure 3). Each degree Celsius increase in temperature in data centers reduces associated cooling costs by about 7 percent, so reducing case size and allowing equipment including power supplies to run hotter can make real savings while freeing up rack space.

Figure 3: Equipment reliability with air inlet temperature. (Source: ASHRAE)
Another enabler for smaller power supplies running hotter is the use of WBG semiconductors fabricated in SiC or GaN materials. These devices have much higher operating temperature ratings than silicon types, particularly SiC, with an allowed die temperature of up to several hundred degrees Celsius.
The Importance of the Power Density Metric
Competing suppliers of power conversion equipment in the industry can vie with each other for claimed efficiencies under very specific conditions, but what matters to the end user is productivity and the profitability of their process. Saving a few dollars by consuming less energy is a good thing, but the dollars earned by increasing the density of equipment in a cabinet or rack and improving productivity per cubic foot might be more attractive. Floor space in data centers and the manufacturing industry has a "dollar density" — a monetary value it must achieve to contribute to revenue — measured in thousands of dollars/square foot, so downsizing the electronics to give more productive space is a real gain (Figure 4). If it means putting off provision of a complete extra cabinet when an expansion is needed, even more dollars are saved in the short and long term.

Figure 4: Factory floor space has a dollar value. (Source: Mouser)
Achieving higher density of electronics with associated power converters is driving system architects to think of "power density" as an increasingly important metric. However, unlike end-to-end electrical efficiency, the power density of a complete system is not easy to compare, and what do you include? In a typical industrial cabinet there might be switchgear, connectors, chassis-mounted electromagnetic interference (EMI) filters, an AC/DC converter generating an intermediate voltage, high-current bus bars, DC/DC converters locally at the loads, fans and their own power supplies, and mounting hardware. You might even include air-conditioning units. In a controls cabinet, the loads might be external, perhaps motors. In this case, the volume of power conversion equipment is a significant proportion of the overall space, and any savings in size allow more control electronics to be included. Returns diminish though, as more power is needed for the extra equipment added. Controls cabinets might also be limited by the requirement to use standardized hardware such as DIN-rails for equipment mounting, with suppliers launching ever-narrower products and the practicality of input/output connector size often defining the minimum. 30W AC/DCs are now down to about 21mm in width, while 480W parts can be around 48mm wide by 124mm high. Cooling in cabinets, if there is any, can just consist of fans with ill-defined inlet temperatures, so power converters tend to be rated only for operation in high-temperature airflow with no chassis heatsinking. This results in a relatively low value for power conversion density, perhaps 10W to 20W per cubic 25mm.
Data Center Power Converters are Heated by Their Load
In data centers, the architecture of power provision strongly affects power density. The latest trends are toward a 48V backplane bus with point-of-load (POL) converters on each server blade reducing the voltage down to IC levels, often sub-1V. Taken in isolation, the POLs can have dramatic power density — over 15kW per square centimeter — but need significant heatsinking or airflow to survive. The 48V bus can be derived from a rack AC/DC converter, which might have a power density of only around 310W per square centimeter. Alternatively, 380VDC can be provided from an external central source with a conversion to 48V in the rack. With a DC supply and no losses from AC rectification and power factor correction circuitry, this converter can be very efficient and again have a high power density of over 15kW per square centimeter (with adequate cooling). An additional advantage is that energy storage for supply loss or brown-outs can be centralized, unlike with AC/DCs in each rack, which have the overhead of large internal reservoir capacitors for ride-through taking valuable space.
Unlike in industrial manufacturing cabinets, data center loads are the server blades themselves, so each rack can be dissipating 10kW+ internally. This mandates active cooling with tightly controlled, high-speed airflow at low inlet temperatures. This is good news for the power converters — which, with their high efficiency, are only dissipating a fraction of the power of the blades. This allows the use of POLs and bus converters with minimal, if any, external heatsinking, keeping the overall power density high. In reality, a major consideration is to keep heat generated by the blades away from the power converters.
WBG Technology Offers Even Higher Power Density
Power converter designers always have the option to increase efficiency by slowing switching speeds, but this results in larger passive components and consequently a larger case size. Complex resonant converter topologies have allowed higher frequency operation with low losses, but the arrival of SiC and GaN semiconductors has changed the game again with their combination of high speed and low losses. Their ability to operate at higher temperatures reliably allows converter package sizes to reduce even further, pushing power-density figures higher.
Conclusion: Designing for Value
Appropriately balancing the trade-offs and costs between improved power density and better power efficiency ensures that the designer delivers the highest value design for customers. Chasing power conversion efficiency percentage can become a game of diminishing returns unless the improvement results in smaller products, leaving space for the equipment that directly adds to the bottom line. Power density is a useful metric for the converters, but should be compared carefully to include all elements in the system, and can be expected to vary hugely between manufacturing industry cabinets and data center server racks. Choose wisely as you design for value.