Skip to main content

High-Density Backplane Connectors for PCIe Gen 6

Designing High-Density Backplane Connectors for PCIe Gen 6 and Beyond

(Source: chutikan/stock.adobe.com; generated with AI)

Each new generation of computing hardware brings faster processors, denser storage arrays, and higher throughput demands. However, the physical dimensions of rack units and server chassis do not change. Packing new functionality into such small spaces creates a combination of electrical, mechanical, and thermal challenges that engineers must address. The backplane connector is central to addressing these challenges, as it ties together the system’s boards, buses, and interconnects. If designed poorly, these connectors can limit the performance of the entire data center.

Backplane connectors have evolved significantly from the days when the DIN 41612 dominated the industry. Signaling speeds now reach 64 gigatransfers per second (GT/s) per lane under Peripheral Component Interface Express (PCIe) Gen 6, and because PCIe Gen 6 uses PAM4 signaling (encoding 2 bits per symbol), the raw speed is 128 gigabits per second (Gbps), which is the raw bit rate moving across the lane.

At these speeds, designers must model and tune the electrical pathway with the same precision as any high-speed differential trace. In many cases, the connector will be the limiting factor in system performance. As such, it can no longer be treated as a commodity interface, which is why this blog details some of the key aspects to consider when selecting backplane connectors for high-speed computing in the PCIe Gen 6 era and beyond, with particular focus on a backplane solution from Amphenol TCS.

The Challenge of Scaling Connectivity

Designing backplane connectivity for high-performance computing and storage systems depends on preserving signal integrity across multiple board transitions. Each mated pair of contacts introduces discontinuities that alter impedance, create reflections, and increase insertion loss. At lower data rates, these variations are tolerable. However, at the frequencies expected in Gen 6, they are catastrophic. Even minor variations in plating thickness, dielectric composition, or contact geometry can distort the signal’s eye pattern beyond recovery.

As computing systems grow more dense to handle the rise in cloud and enterprise workloads, designers face new tradeoffs. Shorter interconnect paths help reduce electrical loss, but tighter layouts limit airflow and increase coupling between high-speed channels. The result is more heat and a greater risk of crosstalk. Connectors must now route hundreds or even thousands of differential pairs through smaller spaces while maintaining impedance control, low skew, and reliable mechanical performance over many insertion cycles.

The need to deliver power from board to board adds to the complexity of connector design. Each contact within the connector must balance its current-carrying capability with the need to ensure isolation and prevent coupling with nearby signal lines. In high-density connectors, where signal and power contacts are mounted just millimeters apart, providing the necessary isolation while maintaining a compact design is critical.

Electrical Design Considerations

The essential characteristics of a high-speed connector are impedance, insertion loss, return loss, and crosstalk. The total channel budget for insertion loss in PCIe Gen 6 is measured in fractions of a decibel per inch, leaving almost no room for any additional losses caused by the connector.

Maintaining a consistent impedance throughout the entire signal chain is vital. To understand why this is so critical, it helps to compare high-speed signals with direct current (DC). In a DC circuit, efficiency is maintained by simply ensuring that resistance is as low as possible. In contrast, information in a high-speed signal chain is carried as a radio frequency (RF) wave. Changes in impedance, especially abrupt changes, introduce reflections in this wave that can close the signal eye and distort timing margins.

Modern connectors achieve consistency by carefully shaping the signal contact and surrounding ground shields, ensuring that the electromagnetic field is confined and symmetrical. Virtual tools capable of simulating full-wave 3D fields have become a key part of the connector design process. With this advancement, designers can now model the precise field distribution within each pair, allowing them to refine their design before building a physical prototype.

Loss management extends beyond impedance. The skin effect and dielectric losses of the insulating material determine how energy dissipates at high frequencies. Low-loss polymers and high-temperature thermoplastics combine structural rigidity with stable dielectric performance, making them a valuable option in connector design.

Mechanical and Thermal Constraints

The connector’s mechanical design also plays an important role in determining its performance. With the high circuit counts found in the latest backplane applications, even mating and unmating a connector can be difficult. Mating forces can become substantial, and alignment features, such as guideposts, enable large connectors to be mated across a backplane without damaging the pins.

Thermal management has also become a significant concern in connector design. Large connectors can impede airflow, creating localized hot spots that degrade both connector materials and surrounding components. Combined with the high ambient temperatures found in data centers, the connector must become part of the system’s overall thermal architecture. Features like airflow channels or staggered contact arrays help maintain cooling efficiency.

Technology Innovations in Next-Generation Connectors

The demands of PCIe Gen 6 and emerging architectures have pushed connector technology into new territory. Traditional open-pin-field connectors relied on physical spacing to control coupling. To cope with the higher demands of modern systems, the latest connectors now employ integrated ground structures around each differential pair. This geometry sharply reduces crosstalk and enables tighter packing without compromising signal integrity.

System architects need scalability as well as performance. Instead of fixed connector designs, next-generation systems use stackable modules that can be tailored to the signal and power requirements of each application. This approach allows designers to configure backplane layouts for optimal routing and airflow while maintaining uniform electrical characteristics.

Amphenol TCS HD Express Interconnect System

Amphenol TCS HD Express® Interconnect System applies high-speed connector design to meet modern data center demands. Designed for 85Ω differential systems, it delivers PCIe Gen 6 performance while achieving the highest contact density currently available in a backplane connector. Its electrical path is tuned to minimize insertion and return loss across the full Gen 6 frequency range, preserving clean eye diagrams even with tight system margins.

The connector’s modular design allows it to scale from midplane to full backplane configurations, providing engineers with flexibility across server, storage, and telecom architectures. Mechanical guidance and mating features are engineered to provide stability in high-volume production environments, while the housing materials ensure dimensional stability under thermal load. Integrated airflow and impedance control enable the HD Express to handle high density without sacrificing signal quality or cooling.

Conclusion

As computing architectures move into the PCIe Gen 6 era, backplane connectors have evolved from mechanical necessities to critical enablers of system performance. Their design determines how well a platform can balance signal integrity, mechanical precision, and thermal management.

The Amphenol TCS HD Express Interconnect System addresses these challenges through shielded differential paths, advanced materials, and a scalable architecture that maintains reliability at higher data rates and densities. It allows engineers to use the latest trends in density and speed without sacrificing reliability. The HD Express series showcases how backplane connectors have become one of the most sophisticated components in the system.

Author

David Pike is well known across the interconnect industry for his passion and general geekiness. His online name is Connector Geek.