Skip to main content

Bringing Edge AI Control to Robotics

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

Published August 25, 2026

Edge artificial intelligence (AI) is moving beyond background analysis and into machines that must sense, decide, and act in real time. Modern robotics, vision systems, and intelligent automation platforms increasingly perform perception, decision-making, and actuation locally rather than relying on remote cloud resources. In these systems, latency directly affects motion control, inspection timing, and machine responsiveness.

Designing systems capable of local perception, immediate decision-making, and synchronized physical action challenges engineering teams to find hardware that can manage both high-performance AI workloads and deterministic real-time control interfaces. Edge AI single-board computer (SBC) designs can address that gap by bringing compute, connectivity, and control closer to the sensors and actuators that define real-world machine behavior.

This week’s New Tech Tuesdays explores the hardware and software requirements for coordinating local AI inference, industrial input/output (I/O), and latency-sensitive machine control, highlighting how edge AI SBCs help robotics, vision systems, and intelligent automation platforms combine high-performance AI processing with deterministic real-time control on a unified hardware platform.

Coordinating Perception and Latency-Sensitive Control

When designing edge AI systems, the central engineering challenge is coordinating intensive AI inference with deterministic motion control and industrial I/O. Traditionally, designers often separate AI processing hardware from time-sensitive microcontrollers. That split can increase integration complexity, power consumption, board space, and communication latency between perception processing and actuation control.

Robotics and automation systems often run vision, planning, motion control, and safety logic in parallel, which places simultaneous demands on compute performance and physical control. Vision systems rely on high-bandwidth camera connections and local processing, while motion systems use pulse-width modulation (PWM), general-purpose input/output (GPIO), and industrial communication interfaces. Distributed automation and mobile robotic systems may use Controller Area Network Flexible Data-Rate (CAN FD), which extends the payload from 8 bytes in Classical CAN to up to 64 bytes and supports higher data rates during the data phase.

In high-speed intelligent automation, delays between sensing and actuation affect inspection timing, motion response, and overall machine behavior. Deterministic hardware interfaces help ensure that physical outputs remain responsive, even while AI models, vision pipelines, and application software place heavy demand on processing resources.

Standardizing Robotics Workflows

Robot development has historically required extensive custom programming before engineers could address higher-level navigation, perception, or application logic. Modern development increasingly relies on reusable frameworks and software components to reduce that burden.

The Robot Operating System 2 (ROS 2) helps structure robotics software around reusable packages, libraries, tools, and development concepts. For engineering teams, the ROS 2 ecosystem moves more effort toward application development and away from low-level integration. Instead of reinventing every driver, node, and control pathway, developers can build from a more standardized robotics foundation.

Development environments that combine embedded control code, Python scripts, Linux® applications, and AI models also reduce workflow fragmentation. By keeping those resources in a shared environment, teams can move more quickly from early experimentation to functional machine behavior. Reusable robotics software blocks shift engineering effort from repetitive integration work toward application logic.

Managing Industrial I/O Convergence

Industrial automation design is moving toward platforms that combine AI workloads with direct machine-level I/O. Edge AI platforms increasingly interface directly with sensors, motor controllers, industrial networks, and machine-level control systems while running complex perception and inference workloads.

A unified board shortens the design path between AI processing and physical actuation, simplifying early prototyping. Bringing compute and control resources together can also reduce the number of separate hardware modules involved in development, helping engineers evaluate system behavior sooner.

Integration convenience does not replace application-specific validation. Processor loading, thermal behavior, power consumption, camera bandwidth, I/O timing, enclosure constraints, software updates, and safety-related behavior still need to be evaluated at the system level.

The Newest Products for Your Newest Designs®

The Arduino® VENTUNO™ Q Edge AI Single Board Computer (Figure 1) addresses the integration burden of bringing local AI directly into physical control applications. The development platform is designed for robotics, vision systems, and intelligent automation applications that connect perception, decision-making, and action on a single board.

Figure 1: The Arduino VENTUNO Q is purpose-built for robotics and physical actuation, empowering developers to build fully offline, low-latency intelligent systems that can see, understand, and interact with the physical world without relying on cloud computing. (Source: Mouser)

The dual-brain architecture at the core of VENTUNO Q’s combines a Qualcomm Dragonwing™ IQ-8275 processor with an STM32H5F5 microcontroller. The Dragonwing IQ-8275 provides neural processing unit (NPU), central processing unit (CPU), and graphics processing unit (GPU) resources for advanced AI and vision workloads. Meanwhile, the STM32H5F5 microcontroller supports deterministic, real-time control for robotics, motion systems, and industrial interfaces.

For development workflows, the board supports Arduino® App Lab, allowing engineers to work with Arduino sketches, Python, Linux applications, and AI models in one environment. The platform also supports ROS 2 for robotics development, while the Arduino App Lab includes robotics Bricks intended to bundle complex robotic functionality into reusable software components.

Moreover, the board combines 16GB RAM and 64GB expandable storage with three 4-lane MIPI-CSI camera interfaces for vision input. For display and connectivity, this SBC includes MIPI-DSI, HDMI, USB Type-C DisplayPort Alt Mode, Wi-Fi® 6, Bluetooth® 5.3, 2.5Gb Ethernet, USB Type-C, and dual USB Type-A 3.0 ports. Control interfaces include CAN FD, PWM, and deterministic GPIO. Together, these interfaces support the sensing, compute, connectivity, and actuation paths required for responsive edge AI development.

Tuesday’s Takeaway

Edge AI increasingly integrates sensing, inference, communication, and physical control within a single system architecture. Robotics, vision systems, and intelligent automation platforms need local intelligence that can interpret sensor data and trigger reliable action without unnecessary latency.

VENTUNO Q gives engineers a unified development platform that combines AI processing, deterministic control, industrial I/O, ROS 2 support, and Arduino App Lab workflows. For design teams building autonomous machines, evaluation should extend beyond peak AI performance to the full machine loop—sensing, inference, communication, motion, timing, and validation. Ultimately, the value of embedded AI is measured not only by what a system can perceive, but by how reliably and predictably it can act on those insights in real time.

About the Author

Mouser, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.

Profile Photo of Mouser Technical Content Staff