Advantech's EPC-R3720 Box Computer Extends Windows on Arm® Ecosystem
A Match Made for Edge Innovation
New Tech Tuesdays
Join Rudy Ramos for a weekly look at all things interesting, new, and noteworthy for design engineers.
Published June 25, 2024
This week’s New Tech Tuesday showcases a cutting-edge solution for edge artificial intelligence (AI) innovation from Advantech.
The Newest Products for Your Newest Designs®
The Advantech EPC-R3720 Edge AI Box Dev Kit (Figure 1) represents a pivotal step forward in the evolution of the Windows on Arm® ecosystem. As the demand for seamless and efficient application development increases, the arrival of such advanced hardware platforms ushers in an era of innovation. Windows on Arm distinguishes itself from traditional Windows laptops through exceptional battery longevity, always-on connectivity, swift boot times, and native security features, thanks to sophisticated chipset integration. The EPC-R3720, specifically designed for industrial automation, healthcare, and application development, is a testament to this evolution.


Figure 1: Advantech's EPC-R3720 Edge AI Box features a high-performance integrated neural processing unit (NPU), facilitating sophisticated machine learning algorithms on edge for minimized latency and bandwidth use. (Source: Advantech)
Embracing the Future with Windows on Arm
Arm's architecture has revolutionized how we think about computing power and efficiency. In this competitive landscape of development kits, the Advantech EPC-R3720 emerges as a crucial component, empowering developers to leverage the inherent advantages of Windows on Arm. The EPC-R3720's design considers the nuanced needs of modern applications, particularly in domains requiring robust processing capabilities alongside energy efficiency and dependable connectivity.
Powering the Next Generation of Applications
The extensive range of applications for the EPC-R3720 demonstrates its adaptability. For instance, industrial automation projects benefit from its robust processing power and high-performance integrated neural processing unit (NPU), facilitating sophisticated machine learning algorithms on edge and minimizing latency and bandwidth use. The device excels in image processing, which is essential for machine vision applications, with efficient video and display capabilities that leverage the Vivante GC7000UL graphics processing unit (GPU). In healthcare, the EPC-R3720 ensures patient data is processed securely and swiftly, enabling real-time monitoring and analytics. For developers, the kit offers a robust platform for Windows on Arm application creation, simplifying the transition from conception to deployment.
Unpacking the Hardware
The EPC-R3720 Edge AI Box Computer is not just another piece of tech; it's the foundation of future-proof systems that demand speed, reliability, security, and value for AI native computing with maximized I/O flexibility for ubiquitous deployments. Pre-loaded with Windows 10 IoT Enterprise on Arm, the EPC-R3720 Edge AI computer offers developers a seamless environment for developing innovative ideas.
The EPC-R3720 offers the following key specifications:
- Processor: NXP Arm Cortex®-A53 i.MX 8M Plus Quad 1.6GHz
- AI Performance: 2.3 TOPS NPU, for real-time inference and accelerated vision-based machine learning at the edge
- Memory: Ample on-board LPDDR4 6GB RAM, 16GB eMMC flash for OS, and 8MB QSPI NOR flash for board information
- Connectivity and Expansion: HDMI up to 3840 × 2160 at 30Hz resolution, dual GbE LAN, USB 2.0, USB 3.2 Gen 1, micro-SD socket, nano SIM slot, mini-PCIe for 3G/4G, M.2 2230 with key E slot
- Enhanced Security: Advanced security features embedded at the chipset level
- High Efficiency: Designed for optimal power management and extended battery life for use in any environment, with a compact 174 × 108 × 25mm fanless design
Tuesday’s Takeaway
Between its versatile applications and its high-performance and efficient design, it's clear that Advantech's EPC-R3720 Edge AI Box is a significant leap forward for the Windows on Arm ecosystem. It is a pivotal, cutting-edge tool for developers and industry professionals seeking to harness Arm-based systems' full potential within the Windows environment. Its strategic focus on crucial sectors such as industrial automation and healthcare underscores its potential to revolutionize how we approach AI and application development on the edge.