Skip to main content

Scaling Edge AI Inference with M.2 Modules

New Tech Tuesdays

Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.

Published November 17, 2026

Artificial intelligence (AI) processing does not always take place in the cloud. Factory equipment can analyze sensor data on site, while inspection cameras can process images as products move through production. Retail systems are also using local processing for certain AI workloads. In these applications, processing data close to its source reduces the amount of information that must travel over the network and eliminates the need to send data to a remote server before a result is returned.[1]

Moving inference to the edge, however, places a processing burden on the local hardware. The system must provide sufficient computing performance for the AI workload without exceeding the device’s power, space, or thermal constraints. As models grow more complex or a system needs to handle several tasks simultaneously, these constraints become even more significant.

Many edge applications run inference continuously. For example, a camera inspecting a production line might analyze images throughout a production shift. Adding another camera or AI model increases the system’s processing requirements. Increasing the processing workload can also increase power consumption and heat generation. In compact embedded equipment, cooling can be limited, so the hardware must maintain the required inference performance within the system's power and thermal limits.

This week's New Tech Tuesdays examines the role of M.2 AI accelerators in edge computing, highlighting how they can expand neural-network processing performance without requiring a complete redesign of existing embedded platforms.

Adding AI Processing at the Edge

One way to handle a growing inference workload is to use a dedicated AI accelerator alongside the host processor. The accelerator handles neural-network processing, while the host processor continues to run the operating system, application software, and other system functions.

One option for adding dedicated AI processing is an M.2 accelerator module. M.2 is a compact module form factor used for devices ranging from storage and wireless connectivity to other types of expansion hardware. In this case, the accelerator plugs into a compatible M.2 socket and communicates with the host over Peripheral Component Interconnect Express (PCIe).[2]

The module must work with the system’s existing hardware and software. Embedded platforms may use x86- or Arm®-based host processors, and developers may create models with frameworks such as TensorFlow or PyTorch, or exchange them using formats such as Open Neural Network Exchange (ONNX). Support for common host architectures and model-development ecosystems can simplify integration, although models must still be translated, optimized, and compiled for the accelerator using a comprehensive software toolchain.

The Newest Products for Your Newest Designs®

For systems that require additional inference performance, Hailo-8 M.2 AI Acceleration Modules provide dedicated AI processing via a standard M.2 socket. The modules use the Hailo-8 processor, which delivers up to 26 trillion operations per second (TOPS), and connect to the host via PCIe Gen 3. Hailo offers M.2 Key M, B+M, and A+E versions to support different host configurations.

The modules support both x86- and Arm-based hosts, as well as Linux and Windows operating systems. Models developed with TensorFlow, TensorFlow Lite, Keras, PyTorch, and ONNX are also supported through Hailo's software tools. This enables engineers to add dedicated inference processing while continuing to use the existing host architecture and development tools.

The Hailo-8 also supports simultaneous processing of multiple streams and models. A system that starts with a single inference workload can use the same accelerator to support additional camera streams or models as processing requirements increase. The modules are available with an extended operating temperature range of -40°C to +85°C for embedded and industrial environments.

Tuesday’s Takeaway

Moving AI inference to the edge places greater processing demands on embedded hardware. Dedicated AI accelerators provide an additional way to handle those workloads without placing the entire burden on the host processor. M.2 modules also offer engineers a compact and scalable method for adding AI processing capabilities to existing platforms as inference requirements continue to grow.

   

Sources

[1]https://www.ibm.com/think/topics/edge-ai
[2]https://pcisig.com/specification-overview/pci-express-m2

About the Author

Mouser, founded in 1964, is a globally authorized distributor of semiconductors and electronic components for over 1,200 industry-leading manufacturer brands. We specialize in the rapid introduction of the newest products and technologies targeting the design engineer and buyer communities. Mouser has 28 offices located around the globe. We conduct business in 23 different languages and 34 currencies. Our global distribution center is equipped with state-of-the-art wireless warehouse management systems that enable us to process orders 24/7, and deliver nearly perfect pick-and-ship operations.

Profile Photo of Mouser Technical Content Staff