Skip to main content

Agentic AI: Automation That Acts on Its Own

(Source: tippapatt/stock.adobe.com)

Artificial intelligence (AI) has moved beyond prediction and chat. The next step is AI systems that can plan and carry out work on their own—within clear limits—so they respond to changing conditions without waiting for a command. This kind of autonomy, known as agentic AI, turns goals into step-by-step plans and executes them through tools and hardware engineers already trust. Incorporating agentic AI results in faster diagnosis of potential issues, fewer handoffs, and steadier operations when conditions drift.

In this blog, we explore how agentic AI is redefining automation across industries by giving systems the ability to develop goals, plan and proactively adjust multi-step strategies, and execute tasks with minimal human input.

What Is Agentic AI?

Agentic AI gives a system the capability to reason about a task and act toward a goal with minimal supervision. Whereas a traditional model answers and stops, in an agentic model, an agent frames the problem, gathers the right inputs, creates a plan, executes through approved interfaces, and checks the result before moving on. In practice, it can work across tasks, prioritize based on objectives, break problems into workable steps, and carry those steps out safely in software and hardware. In a manufacturing plant, for example, an agent can watch sensors in real time, spot an anomaly, review maintenance notes, predict likely faults, and either raise a targeted alert or schedule service in the next allowable window. While people remain in charge of high-impact decisions, the agent handles the planning and follow-through.

Why Engineers Should Pay Attention

For embedded, automation, and test teams, agentic AI changes how systems run day-to-day. Devices at the edge can decide when to run diagnostics based on live signals, and lines can adjust parameters to protect throughput and quality. Procurement agents can adapt sourcing in real time by querying distributor application programming interfaces (APIs) to balance availability, lead time, and cost. The aim is not to replace oversight, but to free engineers from routine coordination so they can focus on design, improvement, and safety. Because agents run on familiar microcontrollers, gateways, and software, adoption can be incremental rather than a complete redesign.

Agent-to-Agent Collaboration: Smarter Together

Transmitting data is not enough when goals span multiple systems. Agent-to-agent (A2A) protocols allow for agentic collaboration, enabling software peers to plan together, verify results, and adapt as conditions change. On a packaging line, one agent watches for vibration and raises an alert when it sees an unusual pattern. A second runs a safe diagnostic routine on the controller, confirms the issue, and narrows the likely cause. A third schedules a repair during a planned stop and checks for distributors’ parts and lead times. If the confirmation is weak, the plan updates: diagnostics expands its checks, monitoring tightens thresholds, and procurement waits. Agents coordinate roles up front, validate each handoff, and revise the plan when the environment shifts. In plants, that coordination often rides over a single, structured interface, such as Open Platform Communications Unified Architecture (OPC UA) for control, while inventory checks employ a well-documented web API for available parts.

Multi-Capability Platforms: Enabling Real Intelligence

A multi-capability platform ties the pieces together so an agent can sense, remember, decide, and act as one system. The platform gathers signals from machines and software and normalizes them so the agent sees a consistent picture. It also maintains both short-term context and a more extended history, allowing today’s behavior to be compared with last week’s. These multi-capability platforms turn goals and observations into a clear plan that other systems can review, then the platform executes only through approved adapters while recording what happened for audit and rollback. Whether the platform runs near the machines, in the cloud, or both, the result is consistent behavior that is easy to verify.

Why It’s Happening Now

Three technological shifts make this emergence of agentic AI practical. One, modern language models can write well-structured plans and pick from a defined tool set, so every step can be checked before it’s run and logged for review. Two, today’s automation environments are more accessible through documented APIs, enabling agents to gather context and act without brittle workarounds. Three, more computation now sits near the machines on gateways and small devices, so routine decisions are fast and resilient even when the network is noisy. Lightweight workflow engines tie planning, action, and verification into one traceable loop, allowing teams to add autonomy in small, safe increments.

Engineering Use Cases Emerging Today

Early wins for agentic AI follow clear patterns. In test and quality assurance (QA), agents watch measurement trends, flag drift, propose a minor, safe experiment, run it under a preapproved routine, and generate a report that links instruments, fixtures, and lots, so engineers can act quickly. In maintenance, agents track signals such as vibration or current, draft a diagnostic plan that stays within safe limits, and, when evidence is strong, schedule work for the next planned window rather than wait for a failure.

Firmware updates become more adaptive as edge devices request, verify, and install changes only when a new threat or protocol shift is detected, delaying or rolling back the update if conditions aren’t right. On the supply side, agents forecast demand from real usage, check distributor data for stock, alternates, and lead times and either place a low-risk order or route a change that touches form, fit, or function for engineering approval with a brief impact note. In smart facilities, multiple agents use A2A protocols to coordinate temperature, motion, and energy use by sharing context, agreeing on a plan, and checking results against site goals, turning one-off optimizations into a continuous loop.

The Road Ahead: Opportunities and Challenges

Agentic AI will expand in two directions. Reusable, task-specific agents will be shared much like apps, and lighter libraries will bring autonomy onto smaller, low-power devices so more intelligence can live at the edge. At the same time, orchestration layers will give operations one place to deploy, monitor, and approve large fleets under shared policies. The risks are clear. Autonomy widens the attack surface, so access should follow the principle of least privilege (PoLP) and changes must be logged and reviewable. Reasoning errors can cascade if checks are weak, which makes plan validation, confidence thresholds, and safe fallbacks essential. Accountability matters in regulated settings, so approvals, provenance, and clean handoffs between people and agents need to be part of the design. The engineering shift here includes building collaboration and governance around control logic so agents deliver speed and adaptability without compromising safety or trust.

Conclusion

Agentic AI is more than a technical upgrade; it’s a shift in how systems learn, interact, plan, adjust, and execute complex workflows. This automation shift offers a practical way to make systems operate faster and with more resilience—without giving up control. Systems diagnose issues sooner, coordinate routine work on their own, and adapt when conditions change. The method is simple: write actions as clear, verifiable plans, execute only through approved interfaces, record what happened, and keep authority bounded so high-impact steps still require human approval. Start with one task on one asset and expand as results earn trust. Because agents use the same APIs and hardware already in a developer’s stack, they can be added incrementally. When parts are needed, agents can query distributor services for stock, alternatives, and lead times. Treated this way, autonomy extends the systems that developers already trust, improving reliability and responsiveness while preserving traceability and a safe path back.

About the Author

With over 10 years of experience in architecting, building, and scaling large-scale machine learning solutions both on-prem and in the cloud, Robert Dempsey specializes in transforming AI strategies into impactful results. He's successfully led multiple large companies in implementing robust AI architectures, and currently leads four data teams as an AI Project Manager at ECS's Justice & Homeland Solutions division. Known for a data-driven approach to problem-solving, he brings a strong mix of technical and strategic skills to drive efficiency, scalability, and innovation across complex ML projects.

Profile Photo of Robert Dempsey