Skip to main content

Communications in Space: A Deep Subject

Transmitting and receiving radio signals between spacecraft in deep space is a snap compared with getting those signals back to Earth, especially when the spacecraft is 120 billion miles away.

Even though we’ve sent spacecraft hundreds of billions of miles into space and rovers are gathering enlightening information about planets, moons, and even asteroids, radio communication in space still remains the new frontier. While the missions themselves are a marvel of technical wizardry, so too is the Herculean feat of not just communicating between spacecraft but sending signals back to Earth.

Communications in Space: A Deep Subject Figure 1

Figure 1: The Pale Blue Dot is part of the first-ever 'portrait' of the solar system taken by Voyager 1. The spacecraft acquired 60 frames to create a mosaic of the solar system from more than 4 billion miles from Earth. At that distance, Earth is just a speck of light less than a pixel in size.

Man’s greatest achievement in this regard is the Voyager spacecraft launched in 1977, that 38 years later is still communicating with Earth from more than 120 billion miles away, and has far outlived even the most optimistic projections of longevity. NASA recently celebrated the 25th anniversary of the last time Voyager sent its last images to Earth in 1990. The decision to take one last glimpse as Voyager left the solar system was made by Carl Sagan, who was a member of the Voyager team. The image (Figure 1) was called “The Pale Blue Dot” and become the title of Sagan’s 1994 book.

Voyager has remained operational for nearly four decades, which is hard enough for Earth-bound electronic systems. It’s a true engineering marvel considering that Voyager technology was state of the art when All in the Family was the TV top sitcom in the U.S. It’s also testament to the incredible capabilities of the NASA Deep Space Network (DSN) that captures Voyager’s incredibly faint radio signal after being weakened by passage through the Earth’s attenuating atmosphere. The space communications challenge is great today, even with technology that is orders of magnitude more advanced. It becomes even more vexing as the resolution of still images and video is far greater, which translates into huge amounts of data from cameras, telescopes, and scientific equipment.

 

 

The Deep Space Network

Communications in Space: A Deep Subject Figure 2

Figure 2: The 70-m antenna at the Goldstone Deep Space Communications Complex, in the Mojave Desert. (Source: "Goldstone DSN antenna". Licensed under Public Domain via Wikimedia Commons.)

In the U.S., the bulk of the development in deep-space communications has been conducted at NASA’s Jet Propulsion Laboratory (JPL) located in La Cañada Flintridge, CA, which is managed for NASA by the California Institute of Technology. The list of advancements achieved by JPL is massive thanks in no small measure to the many scientists who have made contributions there, including Erwin Schrödinger, Werner Heisenberg, Hendrik Lorentz, Niels Bohr, and Albert Einstein. JPL has been a major participant in every NASA space mission, from construction and operation of robotic planetary spacecraft through Earth-orbit and astronomy missions and operation of the DSN that is the terrestrial portion of U.S. deep space mission communications.

The DSN consists of three transmission and reception facilities: the Goldstone Deep Space Communications Complex near Barstow, CA (Figure 2), the Madrid (Spain) Deep Space Communication Complex, and the Canberra (Australia) Deep Space Communication Complex.

They are spaced about 120 deg. apart on the globe in order to provide continuous coverage (Figure 3). To continue meeting the increasing demand on deep space communications systems, NASA believes the DSN must increase its capability by more than a factor of 10 during each of the coming three decades, with a goal of achieving data rates of 200 Mb/s by 2022 and 20 Gb/s by 2030.

Communications in Space: A Deep Subject Figure 3

Figure 3: View from the North Pole showing the field of view of the main DSN antenna locations. Once a mission gets more than 18,600 miles from Earth, it is always in view of at least one of the stations. (2)

Getting Down to Earth

There are basically two elements that comprise deep space communications: transmitting and receiving signals first in space and then through the ionosphere and troposphere that surround Earth. Space is a vacuum, so signals within it are not reduced in strength and once transmitted, will theoretically continue to propagate to whomever (or whatever) might be listening.

This makes it possible to use transmitters that need only generate relatively low RF power, aided immeasurably by very-high-gain antennas on Earth; and terminals like those of the DSN that increase strength of the received signal and amplify the signal transmitted from Earth to the spacecraft. The lack of signal attenuation in space is an enormous benefit, as the small transmitters on spacecraft need produce much less RF power (boosted again by their high-gain antennas) so they consume little DC power, of which there is little to spare on a spacecraft powered by solar cells.

Unlike communication in space, communicating between deep space and Earth is far more difficult, as Earth is surrounded by an atmosphere that consists of five layers, each with different characteristics, but all forming an impediment to radio and optical communications. The atmospheric layers absorb and scatter signals within them, reducing signal strength and limiting the specific portions of the electromagnetic spectrum that can be used for communication. Below 30 MHz, the ionosphere layer of the atmosphere absorbs and reflects signals, and above 30 GHz the lower atmosphere or troposphere absorbs them. As a result the region between (roughly) 30 MHz and 30 GHz is chosen for communications from deep space to Earth.

Having passed through the atmosphere, these signals are invariably reduced in strength and so weak that they can only be received by huge parabolic antennas that generate very high levels of gain, along with receivers with exceptionally low system noise levels. To increase sensitivity even further, these antennas can be combined to produce a single huge aperture that increases the likelihood of reception. Without them, communications form deep space would be impossible.

The Data Dilemma

Deep space missions generate lots of publicity, possibly due to the stunning, high-resolution still images and video. And as all of us who have data-limited wireless plans know, high-resolution means high data rates and “big data”. The imagers, along with scientific instruments, produce more and more data with each mission, thus deep space communications networks must continually be enhanced to accommodate it.

For example, as of 2013 the Mars Reconnaissance Orbiter (MRO) sent about 25 Tbytes of data back to Earth, but NASA estimates this must dramatically increase and along with it the ability to download it to Earth. According to JPL, at its data rate of 5.2 Mb/s, MRO requires 7.5 hours to transmit scientific data stored on its recorder, and 1.5 hours to send a single High Resolution Imaging Science Experiment (HiRISE) image to Earth. HiRISE is the largest camera ever used on any deep space mission, and is mounted on the MRO that was built under the direction of the University of Arizona by Ball Aerospace. As it photographs Mars, it can resolve objects of about 1 foot in size (at 0.3m/pixel) on the planet surface from its place in orbit. HiRISE has imaged Mars landers on the surface, including Curiosity and Opportunity.

High-resolution hyperspectral imagers are one of the greatest contributors to this glut of data as they an image at hundreds or thousands of wavelengths simultaneously, revealing mineral content or other characteristics that cannot be revealed from a single visible-wavelength image. A hyperspectral image is hundreds or thousands of times larger. New image compression technology is being developed to reduce this data to a more manageable size.

The Future Is Optical

The channel capacity of interplanetary RF communications systems has expanded by eight orders of magnitude since 1960, and the resolution that can be achieved in tracking a spacecraft has been improved by a factor of 105. This is been achieved by increasing the efficiency and gain of the transmitters and antennas and by reducing the loss introduced by various RF and microwave components. However, there are limits to what microwave communications systems can achieve in terms of data rate increases within the constraints of mass, power, and volume dictated by the spacecraft.

Nevertheless, NASA has been developing a system called the Reconfigurable Wideband Ground Receiver (RWGR) that will leapfrog the performance of the existing DSN receiver. It is a variable-data-rate, reprogrammable, software-defined radio using an intermediate frequency (IF) sampling receiver that operates at a fixed sampling rate of 1.28 GHz with a 500 MHz instantaneous receive bandwidth. The current receiver samples at a 160 MHz rate and has a bandwidth of 72 MHz. NASA ultimately hopes to achieve telemetry data rates in excess of 1 Gb/s using this system.

Communications in Space: A Deep Subject Figure 4

Figure 4: Block diagram of NASA’s Reconfigurable Wideband Ground Receiver (3)

Even with such advances, JPL predicts that in the future there will be a need to transition from microwave to optical communications, as orders-of-magnitude increases in performance can be achieved within the same levels of power consumption and equipment size. The equipment designed for this purpose is being developed now in order to enable streaming video and data communications over immense distances.

By using the narrow beam of an optical carrier frequency near 200 THz (1550 nm) for transmission, optical communications has the potential to increase the achievable data rate from spacecraft at planetary distances by orders of magnitude with a spacecraft transceiver that is of similar mass and power consumption to a wide beamwidth 32-GHz (Ka band) spacecraft transceiver.

The beamwidth of a microwave communications signal transmitted from Mars is also 100 to 200 times the diameter of the Earth, while an optical communication systems beamwidth is 1/10th to 1/20th of our planet’s diameter, so it is inherently narrower when it reaches Earth. However, with a beamwidth this narrow, the laser beam must target a point with exceptional precision. A narrower beamwidth translates to a 10 to 100 times increase in the power transmitted by the spacecraft to the Earth terminal than is possible with today’s microwave antennas, with additional benefit of a significant reduction in weight and a 99% reduction in the amount of space occupied. And as is presently accomplished with optical communications over fiber optics, there is virtually no limit to the amount of available bandwidth, so almost any amount of data can be accommodated. Development of such systems is far from trivial and will require laser transmitters that are exceptionally efficient, can withstand the hostile environment of space, are reliable enough to perform over a system’s operational life of a decade or more, are sensitive enough to receive the faint signals visible during daylight hours, and can function reliably in deep space.

Making Do with Technology We Already Have

JPL as well as other space science organizations throughout the world are working on ways to meet the needs of high-data-rate deep space communications and ultimately the needs of manned spacecraft once they are capable of leaving the solar system. JPL has already spent decades developing power-efficient channel codes that achieve reliable transmission from deep space to Earth, and they are currently so effective they can achieve data rates near the theoretical (Shannon) limit. Technologies in development include channel coding that makes communication possible over otherwise unusable channels by adding redundancy. This could make the transmitted message 100% recoverable even in the presence of massive levels of noise and data corruption.

Low-density parity-check (LDPC) codes have been created that have maximum data rates above 1 Gb/s using current FPGA technology. For the most distant missions to outer planets or beyond the Solar System, JPL has designed “turbo codes” that can operate on channels whose noise power is more than five times higher than the signal power. LDPC and turbo codes, along with protocols for variable-coded modulation (VCM) that vary the channel codes and modulation from code block to code block, may be able to double the data return of a mission without any hardware changes.

While increasing data rates is exceptionally important, it is also necessary to compress data as much as possible to reduce volume. Standard compression algorithms such as JPEG take too much computing horsepower to be suitable for use on a spacecraft, so JPL is using a technique called ICER image compression. It achieves the same result but is much less complex and requires less formidable signal processing hardware. It has already been used on the Spirit and Opportunity Mars rovers to return images of high quality using a compression ratio of 10:1.

The Major Challenges Ahead

If one thing of certainty can be said of future space exploration, it is that we will reach further and further from Earth. Among the hundreds of other challenges posed by this adventure are those associated with communicating with, and receiving images and other data, from spacecraft. That will require exploring new approaches such as the use of free-space optical communications, greater data compression and new data coding schemes, and others that together will together propel us to where no man has gone before.

References

  1. NASA
  2. NASA/JPL
  3. DSNantenna" by "SimonOrJ, Licensed under Public Domain via Wikimedia Commons
  4. Reconfigurable Wideband Ground Receiver Hardware Description and Laboratory Performance, Kenneth S. Andrews, Arby Argueta, et al, California Institute of Technology

About the Author

Barry Manz is president of Manz Communications, Inc., a technical media relations agency he founded in 1987. He has since worked with more than 100 companies in the RF and microwave, defense, test and measurement, semiconductor, embedded systems, lightwave, and other markets. Barry writes articles for print and online trade publications, as well as white papers, application notes, symposium papers, technical references guides, and Web content. He is also a contributing editor for the Journal of Electronic Defense, editor of Military Microwave Digest, co-founder of MilCOTS Digest magazine, and was editor in chief of Microwaves & RF magazine.