Time-Sensitive Networking Delivers Deterministic Industrial Ethernet

New Tech Tuesdays
Join Mouser's Technical Content team for a weekly look at all things interesting, new, and noteworthy for design engineers.
Published May 19, 2026
In the smart factory, information has become as critical as raw materials and energy. Modern production depends on data flowing freely between every layer of an operation, from enterprise scheduling systems down to the sensors and actuators that control machines on the factory floor. This connectivity is central to the Industrial Internet of Things (IIoT). Without it, modern factories can’t adapt quickly or anticipate the problems that can cause downtime.
Once decisions start happening at the edge, network delays become intolerable. Robotics and control systems need timing they can rely on. A delayed packet may be inconvenient in an office network, but in an industrial system, it can compromise safety or stop production.
IIoT requires more than standard Ethernet. It demands networking where time-critical data arrives at guaranteed times, even alongside less critical traffic. With Time-Sensitive Networking (TSN), Ethernet is designed to meet this need, bringing guaranteed bandwidth, ultra-low latency, and precise synchronization to the connected factory.
In this week’s New Tech Tuesdays, we look at why “best-effort” Ethernet falls short for industrial control, how TSN makes Ethernet deterministic, what’s driving adoption now, and what that means for next-generation edge designs.
The Need for Predictable Industrial Ethernet
Conventional Ethernet is very effective for moving large volumes of data, but it is not designed to guarantee when the data will arrive. When a network is busy, data can arrive later than expected or out of sequence. In office networks, that usually just means a short delay.
However, in industrial systems, any delay can cause real problems. When control messages arrive late, machines can fall out of sync or stop altogether. Industrial automation depends on communication that behaves the same way every time, especially for closed-loop control.
To further complicate matters, factories still need to move non-critical data across the same infrastructure. Monitoring and diagnostic data share the network with control traffic. The trick is keeping critical messages predictable without losing the flexibility Ethernet provides. That’s where TSN fits: it keeps a single network usable for many traffic types while protecting time-critical traffic from surprises.
How TSN Works
TSN is a set of Institute of Electrical and Electronics Engineers (IEEE) 802.1 standards that enhance Ethernet with scheduled traffic delivery and precise time synchronization.[1] Critical control data is assigned guaranteed transmission windows, ensuring it arrives reliably and on time, even alongside lower-priority traffic.
This reliability matters most in systems where timing affects behavior. For example, industrial robots rely on coordinated motion, and that coordination depends on control messages arriving when expected. If those messages drift or arrive late, accuracy suffers and robots operate inefficiently or not at all.
TSN also supports advanced smart manufacturing, where sensors, actuators, and edge controllers exchange real-time data to optimize production. TSN-enabled Ethernet supports the flexibility that allows critical and non-critical systems to share the same network without compromising reliability. In practical terms, TSN is often discussed in terms of a few core capabilities. First, it synchronizes time across devices so everything uses the same clock. It also schedules transmission windows for the most time-critical messages and shapes and prioritizes traffic so lower-priority data doesn’t crowd out control communication.
TSN is also becoming important in smart grid and energy infrastructure. Time-critical communication supports real-time monitoring and protection systems across distributed networks, helping energy providers respond faster to faults and load changes.
As Industry 5.0 expands, intelligence is being deployed closer to machines and processes at the network edge. These edge nodes rely on ultra-low latency and predictable connectivity to make real-time decisions while remaining integrated into broader digital systems. In other words, as the edge takes on more responsibility, fast networking is no longer enough—trustworthy timing is the new demand.
What’s Changing Now?
Deterministic networking has always been important in industrial automation, but its use is changing. For example, control traffic, monitoring data, and high-level system communications are expected to share the same network rather than run on separate infrastructure, therefore placing higher demands on timing and predictability.[2]
In factories where intelligence is moving closer to machines, network behavior can influence how systems are designed. Edge controllers and coordinated machines rely on consistent communication timing to make real-time decisions.[3] TSN allows that predictability to exist within standard Ethernet, rather than requiring dedicated networks for control traffic. This shift can simplify network design by allowing factories to use fewer separate networks while still providing the predictable timing that control systems require.
This approach is also appearing in other emerging areas, like smart grids and energy infrastructure, since delayed communication can affect protection and coordination functions.[4] Predictable Ethernet is becoming more of a practical requirement as industrial systems scale and become more interconnected.
The Newest Products for Your Newest Designs®
The STMicroelectronics Nucleo-N657X0-Q board provides a development platform for next-generation industrial edge applications. The board, designed to support high-performance embedded processing, enables engineers to prototype intelligent endpoints that operate within connected industrial environments.
As TSN-enabled Ethernet becomes the foundation for deterministic industrial communication, platforms such as the Nucleo-N657X0-Q help developers create edge controllers capable of real-time responsiveness, secure connectivity, and integration into smart factory networks.
By supporting advanced embedded workloads at the network edge, these development solutions play an important role in scalable industrial automation and future-ready infrastructure.
Tuesday’s Takeaway
Industrial automation depends on networks with predictable communication as well as speed. Control systems need communication that arrives when expected. TSN extends Ethernet to support predictable timing and low latency, making it suitable for industrial control systems that depend on reliable, real-time communication. As IIoT pushes intelligence toward the edge and more traffic types share the same wires, TSN helps Ethernet behave consistently. This reliability enables factories to connect more systems without sacrificing control performance.
Sources
[1]https://standards.ieee.org/products-programs/time-sensitive-networking/
[2]https://www.controleng.com/how-tsn-benefits-industrial-applications/
[3]https://www.controleng.com/why-time-sensitive-networking-tsn-is-the-backbone-of-next-gen-digital-manufacturing
[4]https://www.isa.org/intech-home/2018/november-december/features/time-sensitive-networking-in-automation