Weird RF Part 2: Removing Obstacles to Space Travel
Bounce radio signals off the moon? Unthinkable! Well it certainly was in 1945, when scientists at the U. S. Army Signal Corps at Fort Monmouth (Wall Twp., NJ) resuming trying (after World War II ended) to pierce the Earth's ionosphere with electromagnetic energy. Hardly anyone knew much about this program called “Project Diana” (named for the Greek goddess of the moon), and many still don’t today. This is a shame, as the project and its key participant removed one of the greatest obstacles to space travel.
In 1945 it was believed that RF energy could not penetrate the ionosphere thus making communication between Earth and space impossible. Without the ability to communicate between Earth and manned or unmanned spacecraft, space exploration was also off the table. In 1945, one way to know for sure that this was true was to transmit a high-energy signal directly at the moon and measure whatever (if any) reflections were detected.
But there was fundamental obstacle: No one had determined the velocity of a point on the moon relative to a point on Earth. Enter mathematician and physicist Dr. Walter S. McAfee, who worked at Ft. Monmouth’s Electronics Research Command. After hundreds of hours of calculations, he ultimately determined the answer, a feat that eliminated the barrier to conducting the experiment.
Lt. Col. John DeWitt and chief scientist E. King Stodola, accompanied by a few radar researchers, modified a ‘bedspring’ radar antenna to deliver 24 dB of forward gain, a transmitter to produce 3 kW at 111.5 MHz in 250-ms pulses, and a receiver that compensated for Doppler modulation of the reflected signal. Since the antenna could be rotated only in azimuth and not in elevation, attempts could only be made as the moon passed through the 15°-wide beam at moonrise and moonset. This meant that there were only 40 minutes of observation on each pass as the moon transited the various lobes of the antenna pattern.
On the morning of January 10, 1964, the team aimed the antenna at the rising moon and transmitted a series of radar signals. To their delight the first successful echo detection appeared at 11:58 am EST and the echo was received in exactly 2.5 seconds—exactly as McAfee had calculated! Ten years later, the era of spaceflight began.

Oscilloscope display of the radar signals: transmitted signal on the left and radar return on the right. The arrow at right shows the distance in miles to the moon.
In 2011, nearly a century after its creation and after hundreds of breakthroughs, the 1,126-acre Ft. Monmouth, a.k.a. “Soul of the Signal Corps”, was shut down as part of the Base Alignment and Closure (BRC) program and its equipment and many of its employees were reassigned to various posts. After an audit, the $100 million in savings predicted by the Army was actually determined to be a paltry $31 million.
Sadly, announcements of the Project Diana breakthrough did not include McAfee's name, nor was there any recognition of his role until many years later, and his contribution is still not widely known. The Wikipedia Project Diana page doesn’t mention him. Today, the Project Diana site is maintained by the Ocean-Monmouth Amateur Radio Club as part of the Infoage Science/History Learning Center.